Post Go back to editing

AD9364 Tx attenuation steps error

Thread Summary

The user encountered an issue where the maximum TX power on their custom board based on FMCOMMS4EBZ occurred at 20 dB attenuation instead of 0 dB. The solution involved adding a DC bias to the TX output differential port, which normalized the attenuation behavior. The AD7291 was confirmed not to be the cause of the issue. The power levels were measured at 4.73 GHz, and the custom board's output power was -18 dBm at 20 dB attenuation, -38 to -40 dBm at 0 and 40 dB attenuation, respectively.
AI Generated Content
Category: Hardware
Product Number: AD9364
Software Version: ADI IIO Head-gac3f5db

Hi,

We are developing a hardware from the FMCOMMS4EBZ. We copied the hardware except the AD7291 and defined the pin assignment as the same as FMCOMMS4 to connect with Zedboard. Finally we compared with our board and FMCOMMS4 and found a strange thing.

When we set TX attenuation by FMCOMMS4EBZ, the max power of FMCOMMS4EBZ measured at attenuation 0. This is correct and makes sense.

But when set TX attenuation by our board, the max power of our board happend at  attenuation 20. This is very strange. When I changed the attenuation from 20 to 0, the power reduced 20 dB. Or I changed attenuation from 20 to 0 and the power reduced 20 dB , too. The attenuation should be related to SPI control only and I have no idea why this happend?

best regards

Parents Reply Children