Post Go back to editing

fastlock profile with more than 8 profile saving.

Hello everyone!

I have been working with fastlock profile and I wanted to use more than 8 profile to hope the frequency.now i'm able to recall 8 profile,but i'm not getting what to do if I wanted to use more than 8 profile as i'm using your --> ad9361_fastlock_save(phy, 1, profile, values); function to save more that 8 profile. if i'm going to use more than 8 frequency then while recalling only last  8 frequency are coming instead of that I want continuous chian.

my sequence of execution is :     set_lo_tx --> store  --> load --> save  --> recall

Parents
  • Hi 

    Before posting this doubt I have gone through above link , but still I need clarity about the procedure . Can you please help me with a example code which will help me to set more than 8 profiles.

    Thanks in advance 

    regards,

  • Attached is the code for setting more than 8 profiles:

    cd /sys/bus/iio/devices/iio\:device1/
    pwd
    for i in {1..8..1}
    do
       echo $((650000000 + $i * 100000000)) > out_altvoltage1_TX_LO_frequency
       sleep 0.1
       echo $i > out_altvoltage1_TX_LO_fastlock_store
       echo $i > out_altvoltage1_TX_LO_fastlock_save
       cat out_altvoltage1_TX_LO_fastlock_save
       cat out_altvoltage1_TX_LO_frequency
    done
    for i in {9..16..1}
    do
       echo $((1000000000 + $i * 200000000)) > out_altvoltage1_TX_LO_frequency
       echo $i > out_altvoltage1_TX_LO_fastlock_store
       echo $i > out_altvoltage1_TX_LO_fastlock_save  
       cat out_altvoltage1_TX_LO_fastlock_save
       cat out_altvoltage1_TX_LO_frequency 
    done
    echo 1 150,0,0,0,0,65,23,7,238,85,111,221,115,252,12,160 > out_altvoltage1_TX_LO_fastlock_load
    echo 2 85,0,0,0,0,114,31,15,238,85,111,221,114,221,43,183 > out_altvoltage1_TX_LO_fastlock_load
    echo 3 95,0,0,0,0,113,16,16,238,85,111,221,114,204,217,166 > out_altvoltage1_TX_LO_fastlock_load
    echo 4 105,0,0,0,0,113,31,15,238,85,127,221,114,204,154,176 > out_altvoltage1_TX_LO_fastlock_load
    echo 5 115,0,0,0,0,97,29,13,238,85,111,221,114,204,108,192 > out_altvoltage1_TX_LO_fastlock_load
    echo 6 125,0,0,0,0,97,27,11,238,85,111,221,114,236,73,160 > out_altvoltage1_TX_LO_fastlock_load
    echo 7 135,0,0,0,0,65,25,9,238,85,111,221,114,252,44,198 > out_altvoltage1_TX_LO_fastlock_load
    echo 8 145,0,0,0,0,65,23,7,238,68,110,238,114,252,22,166 > out_altvoltage1_TX_LO_fastlock_load
    echo "recalling first 8 profiles"
    for i in {1..8..1}
    do 
        echo $i > out_altvoltage1_TX_LO_fastlock_recall
        cat out_altvoltage1_TX_LO_frequency
    done 
    echo 9 140,0,0,0,0,65,24,8,238,85,110,221,113,252,32,192 > out_altvoltage1_TX_LO_fastlock_load
    echo 10 150,0,0,0,0,65,23,7,238,85,111,221,113,252,12,160 > out_altvoltage1_TX_LO_fastlock_load
    echo 11 80,0,0,0,0,114,31,15,238,85,111,221,112,253,99,163 > out_altvoltage1_TX_LO_fastlock_load
    echo 12 85,0,0,0,0,114,31,15,238,85,111,221,112,221,43,18 > out_altvoltage1_TX_LO_fastlock_load
    echo 13 90,0,0,0,0,114,30,14,238,85,111,221,112,237,253,1824 > out_altvoltage1_TX_LO_fastlock_load
    echo 14 95,0,0,0,0,113,16,16,238,85,111,221,112,204,217,166 > out_altvoltage1_TX_LO_fastlock_load
    echo 15 100,0,0,0,0,113,31,15,238,85,111,221,112,204,183,176 > out_altvoltage1_TX_LO_fastlock_load
    echo 16 105,0,0,0,0,113,31,15,238,85,127,221,112,204,155,176 > out_altvoltage1_TX_LO_fastlock_load
    echo "recalling 9-16 profiles" 
    for i in {9..16..1}
    do 
        echo $i > out_altvoltage1_TX_LO_fastlock_recall
        cat out_altvoltage1_TX_LO_frequency
    done 

Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.