Post Go back to editing

Initialization of ad9361

Category: Software
Product Number: ad9361
Software Version: no-Os

Hi,

I would like to ask:

1) Is there a tool that can have freq, bandwidth, sampling rate, gain, as inputs and produce the series of SPI register values that are needed to initialize the ad9361 as an output?

2) If there is not such tool, is there a way to build the no-OS driver for ad9361 without any platform (Xilinx, altera,...) to achieve this goal?

Thanks,

Parents
  • 1) Is there a tool that can have freq, bandwidth, sampling rate, gain, as inputs and produce the series of SPI register values that are needed to initialize the ad9361 as an output?

    we don't have such tool and also it is not recommended to initialize the ad9361 chip with SPI register values alone.

    2) If there is not such tool, is there a way to build the no-OS driver for ad9361 without any platform (Xilinx, altera,...) to achieve this goal?

    There should a platform to built the drivers, You can refer to this Building HDL [Analog Devices Wiki]

Reply
  • 1) Is there a tool that can have freq, bandwidth, sampling rate, gain, as inputs and produce the series of SPI register values that are needed to initialize the ad9361 as an output?

    we don't have such tool and also it is not recommended to initialize the ad9361 chip with SPI register values alone.

    2) If there is not such tool, is there a way to build the no-OS driver for ad9361 without any platform (Xilinx, altera,...) to achieve this goal?

    There should a platform to built the drivers, You can refer to this Building HDL [Analog Devices Wiki]

Children
No Data