Hello all,
Vivado 2017.1
SDK no-os
I need to receive a signal on RX1A, process it, then send it on TX1A . I successfully implemented the receiver side, but this is the first time trying to use the ad9361 transmitter.
To make things easy, I am trying to receive the signal and transmit it as is (without processing for now), so I thought I would just need to route the signals in the FPGA as shown in the attached graph...unfortunately, I am not getting the signal at the transmitter ?
Note: on the no-os side, I am using the same configurations (LO frequency, clocks, FIR, etc) for both RX and TX.
Am I routing the correct signals in the FPGA or I need additional signals (valid, etc)?
Regards,
Murad