Post Go back to editing

Kernel Crash on ZCU102 When Initializing ADRV904x

Category: Software
Product Number: adrv904x
Software Version: koror_dev

Hi,

I am trying to bring up the ADRV904X using the ZCU102 evaluation board. To generate the boot files, I followed the steps described in the official wikis as well as the solution provided in the following forum thread:

https://ez.analog.com/linux-software-drivers/f/q-a/599666/boot-files-and-kernel-support-of-zcu102-evaluation-board-with-adrv904x/586706

The boot files are generated successfully, but when I try to boot the board using these files, the system crashes during boot and does not complete execution. The kernel ends up with the following call trace:

[   16.445794] Call trace:
[   16.445796]  dump_backtrace+0x94/0xec
[   16.445806]  show_stack+0x18/0x24
[   16.445814]  dump_stack_lvl+0x48/0x60
[   16.445822]  dump_stack+0x18/0x24
[   16.445829]  panic+0x2fc/0x350
[   16.445834]  nmi_panic+0x8c/0x90
[   16.445839]  panic_bad_stack+0xe4/0xf0
[   16.445845]  handle_bad_stack+0x34/0xbc
[   16.445853]  __bad_stack+0x78/0x7c
[   16.445858]  update_group_capacity+0x4/0x1dc
[   16.445865]  find_busiest_group+0x48/0x448
[   16.445872]  load_balance+0x240/0x9b8
[   16.445879]  newidle_balance.constprop.0+0x174/0x3e8
[   16.445887]  pick_next_task_fair+0x40/0x354
[   16.445894]  __schedule+0x118/0x7e4
[   16.445902]  schedule+0x50/0xac
[   16.445909]  schedule_timeout+0x8c/0x100
[   16.445916]  __wait_for_common+0xd4/0x230
[   16.445923]  wait_for_completion_timeout+0x20/0x2c
[   16.445931]  spi_transfer_one_message+0x488/0x540
[   16.445939]  __spi_pump_transfer_message+0x190/0x4a8
[   16.445944]  __spi_sync+0x208/0x2d4
[   16.445950]  spi_sync+0x30/0x54
[   16.445955]  spi_sync_transfer.constprop.0+0x78/0xa8
[   16.445966]  linux_adrv904x_SpiRead+0xc4/0x110
[   16.445975]  adrv904x_FlushParse+0x90/0x4b4
[   16.445983]  adi_adrv904x_RegistersByteRead+0x17c/0xdf0
[   16.445989]  adrv904x_CpuMailboxBufferRead+0xb4/0x3b4
[   16.445999]  adrv904x_CpuCmdRespRead+0x120/0xce0
[   16.446008]  adrv904x_CpuCmdSend+0xfc/0x71c
[   16.446016]  adi_adrv904x_InitCalsCheckCompleteGet_v2+0xa0/0x4ac
[   16.446024]  adi_adrv904x_InitCalsWait_v2+0xa8/0x3a4
[   16.446031]  adi_adrv904x_PostMcsInit+0x3e0/0xb24
[   16.446040]  adrv904x_jesd204_setup_stage2+0x70/0xf4
[   16.446047]  jesd204_fsm_table_entry_cb+0x9c/0x138
[   16.446055]  jesd204_fsm_handle_con_cb+0x88/0x2a4
[   16.446061]  __jesd204_fsm+0x3c4/0x5b0
[   16.446066]  jesd204_fsm_table+0x128/0x41c
[   16.446072]  jesd204_fsm_probe_done+0x2c/0x38
[   16.446078]  __jesd204_all_links_fsm_done_cb+0x48/0x114
[   16.446084]  __jesd204_fsm+0x454/0x5b0
[   16.446090]  __jesd204_fsm_start+0xe0/0x124
[   16.446095]  devm_jesd204_fsm_start+0x2c/0xb8
[   16.446101]  axi_jesd204_tx_probe+0x478/0x7b0
[   16.446109]  platform_probe+0x68/0xc4
[   16.446115]  really_probe+0x148/0x2ac
[   16.446123]  __driver_probe_device+0x78/0x12c
[   16.446131]  driver_probe_device+0xd8/0x15c
[   16.446139]  __device_attach_driver+0xb8/0x134
[   16.446147]  bus_for_each_drv+0x84/0xe0
[   16.446154]  __device_attach+0x9c/0x188
[   16.446162]  device_initial_probe+0x14/0x20
[   16.446170]  bus_probe_device+0xac/0xb0
[   16.446177]  deferred_probe_work_func+0x88/0xc0
[   16.446185]  process_one_work+0x138/0x28c
[   16.446193]  worker_thread+0x29c/0x4b8
[   16.446198]  kthread+0xe4/0xe8
[   16.446207]  ret_from_fork+0x10/0x20
[   16.446214] SMP: stopping secondary CPUs
[   16.446220] Kernel Offset: disabled
[   16.446222] CPU features: 0x0,00000008,00020000,0000420b
[   16.446226] Memory Limit: none

I’m not sure whether there is any additional step missing, any file that needs to be added, or any manual configuration required on the boards, since the setup process involves jumping back and forth between several different wikis.

Zynq MP First Stage Boot Loader
Release 2023.2   Jan 14 2026  -  09:18:57
NOTICE:  BL31: Non secure code at 0x8000000
NOTICE:  BL31: v2.12.0(release):xilinx-v2025.1
NOTICE:  BL31: Built : 16:07:28, Jan  8 2026
PMUFW:  v1.1


U-Boot 2018.01-21442-gf06dec3cab (Feb 13 2025 - 17:12:07 +0200) Xilinx ZynqMP ZCU102 revA, Build: jenkins-development-build_uboot-57

I2C:   ready
DRAM:  4 GiB
EL Level:       EL2
Chip ID:        zu9eg
MMC:   sdhci@ff170000: 0 (SD)
*** Warning - bad CRC, using default environment

In:    serial@ff000000
Out:   serial@ff000000
Err:   serial@ff000000
Bootmode: LVL_SHFT_SD_MODE1
Net:   ZYNQ GEM: ff0e0000, phyaddr 15, interface rgmii-id

Warning: ethernet@ff0e0000 using MAC address from ROM
eth0: ethernet@ff0e0000
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
Device: sdhci@ff170000
Manufacturer ID: 9f
OEM: 5449
Name: SDCHE
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 29 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading system.dtb
46050 bytes read in 30 ms (1.5 MiB/s)
reading Image
43610624 bytes read in 2868 ms (14.5 MiB/s)
## Flattened Device Tree blob at 04000000
   Booting using the fdt blob at 0x4000000
   Loading Device Tree to 000000000fff1000, end 000000000ffff3e1 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.6.0 (acbarros@servidorvigo1) (aarch64-xilinx-linux-gcc.real (GCC) 12.2.0, GNU ld (GNU Binutils) 2.39.0.20220819) #1 SMP Wed Jan 14 08:39:29 CET 2026
[    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[    0.000000] printk: bootconsole [cdns0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] OF: reserved mem: 0x000000003ed00000..0x000000003ed3ffff (256 KiB) nomap non-reusable memory@3ed00000
[    0.000000] OF: reserved mem: 0x000000003ef00000..0x000000003ef3ffff (256 KiB) nomap non-reusable memory@3ef00000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000000000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x000000087fffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000000000000-0x000000003ecfffff]
[    0.000000]   node   0: [mem 0x000000003ed00000-0x000000003ed3ffff]
[    0.000000]   node   0: [mem 0x000000003ed40000-0x000000003eefffff]
[    0.000000]   node   0: [mem 0x000000003ef00000-0x000000003ef3ffff]
[    0.000000]   node   0: [mem 0x000000003ef40000-0x000000007fffffff]
[    0.000000]   node   0: [mem 0x0000000800000000-0x000000087fffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000087fffffff]
[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000 on node -1
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 18 pages/cpu s36456 r8192 d29080 u73728
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1032192
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 4.
[    0.000000] software IO TLB: mapped [mem 0x000000006c000000-0x0000000070000000] (64MB)
[    0.000000] Memory: 3741540K/4194304K available (19584K kernel code, 1756K rwdata, 17812K rodata, 3328K init, 719K bss, 190620K reserved, 262144K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x1ffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
[    0.000000] sched_clock: 57 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
[    0.008325] Console: colour dummy device 80x25
[    0.012463] printk: console [tty0] enabled
[    0.016523] printk: bootconsole [cdns0] disabled
[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.6.0 (acbarros@servidorvigo1) (aarch64-xilinx-linux-gcc.real (GCC) 12.2.0, GNU ld (GNU Binutils) 2.39.0.20220819) #1 SMP Wed Jan 14 08:39:29 CET 2026
[    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8')
[    0.000000] printk: bootconsole [cdns0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] OF: reserved mem: 0x000000003ed00000..0x000000003ed3ffff (256 KiB) nomap non-reusable memory@3ed00000
[    0.000000] OF: reserved mem: 0x000000003ef00000..0x000000003ef3ffff (256 KiB) nomap non-reusable memory@3ef00000
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000000000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x000000087fffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000000000000-0x000000003ecfffff]
[    0.000000]   node   0: [mem 0x000000003ed00000-0x000000003ed3ffff]
[    0.000000]   node   0: [mem 0x000000003ed40000-0x000000003eefffff]
[    0.000000]   node   0: [mem 0x000000003ef00000-0x000000003ef3ffff]
[    0.000000]   node   0: [mem 0x000000003ef40000-0x000000007fffffff]
[    0.000000]   node   0: [mem 0x0000000800000000-0x000000087fffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000000000000-0x000000087fffffff]
[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000 on node -1
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.5
[    0.000000] percpu: Embedded 18 pages/cpu s36456 r8192 d29080 u73728
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Kernel command line: earlycon clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1032192
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] software IO TLB: area num 4.
[    0.000000] software IO TLB: mapped [mem 0x000000006c000000-0x0000000070000000] (64MB)
[    0.000000] Memory: 3741540K/4194304K available (19584K kernel code, 1756K rwdata, 17812K rodata, 3328K init, 719K bss, 190620K reserved, 262144K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x1ffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
[    0.000000] sched_clock: 57 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
[    0.008325] Console: colour dummy device 80x25
[    0.012463] printk: console [tty0] enabled
[    0.016523] printk: bootconsole [cdns0] disabled
[    0.021134] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
[    0.021152] pid_max: default: 32768 minimum: 301
[    0.021251] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.021274] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.022497] rcu: Hierarchical SRCU implementation.
[    0.022507] rcu:     Max phase no-delay instances is 1000.
[    0.022805] EFI services will not be available.
[    0.022979] smp: Bringing up secondary CPUs ...
[    0.023363] Detected VIPT I-cache on CPU1
[    0.023424] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.023837] Detected VIPT I-cache on CPU2
[    0.023880] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.024268] Detected VIPT I-cache on CPU3
[    0.024311] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.024362] smp: Brought up 1 node, 4 CPUs
[    0.024399] SMP: Total of 4 processors activated.
[    0.024407] CPU features: detected: 32-bit EL0 Support
[    0.024415] CPU features: detected: CRC32 instructions
[    0.024478] CPU: All CPU(s) started at EL2
[    0.024486] alternatives: applying system-wide alternatives
[    0.026135] devtmpfs: initialized
[    0.031979] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.032003] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.037635] pinctrl core: initialized pinctrl subsystem
[    0.038611] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.039437] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.039558] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.039726] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.039767] audit: initializing netlink subsys (disabled)
[    0.039871] audit: type=2000 audit(0.032:1): state=initialized audit_enabled=0 res=1
[    0.040158] cpuidle: using governor menu
[    0.040247] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.040311] ASID allocator initialised with 65536 entries
[    0.053615] Modules: 21936 pages in range for non-PLT usage
[    0.053623] Modules: 513456 pages in range for PLT usage
[    0.054038] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.054057] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.054068] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.054077] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.054087] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.054096] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.054106] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.054115] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.121279] raid6: neonx8   gen()  2263 MB/s
[    0.189333] raid6: neonx4   gen()  2217 MB/s
[    0.257404] raid6: neonx2   gen()  2123 MB/s
[    0.325469] raid6: neonx1   gen()  1814 MB/s
[    0.393526] raid6: int64x8  gen()  1415 MB/s
[    0.461590] raid6: int64x4  gen()  1568 MB/s
[    0.529650] raid6: int64x2  gen()  1394 MB/s
[    0.597721] raid6: int64x1  gen()  1033 MB/s
[    0.597731] raid6: using algorithm neonx8 gen() 2263 MB/s
[    0.665755] raid6: .... xor() 1653 MB/s, rmw enabled
[    0.665766] raid6: using neon recovery algorithm
[    0.666175] iommu: Default domain type: Translated
[    0.666186] iommu: DMA domain TLB invalidation policy: strict mode
[    0.666397] SCSI subsystem initialized
[    0.666563] usbcore: registered new interface driver usbfs
[    0.666594] usbcore: registered new interface driver hub
[    0.666625] usbcore: registered new device driver usb
[    0.666812] mc: Linux media interface: v0.10
[    0.666850] videodev: Linux video capture interface: v2.00
[    0.666898] pps_core: LinuxPPS API ver. 1 registered
[    0.666908] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.666931] PTP clock support registered
[    0.666967] EDAC MC: Ver: 3.0.0
[    0.667279] zynqmp-ipi-mbox mailbox@ff9905c0: Registered ZynqMP IPI mbox with TX/RX channels.
[    0.667792] jesd204: created con: id=0, topo=0, link=0, /axi/spi@ff040000/ad9528-1@1 <-> /fpga-axi@0/axi-adxcvr-tx@84a80000
[    0.667825] jesd204: created con: id=1, topo=0, link=2, /axi/spi@ff040000/ad9528-1@1 <-> /fpga-axi@0/axi-adxcvr-rx@84a60000
[    0.667855] jesd204: created con: id=2, topo=0, link=0, /fpga-axi@0/axi-adxcvr-tx@84a80000 <-> /fpga-axi@0/axi-jesd204-tx@84a90000
[    0.667882] jesd204: created con: id=3, topo=0, link=2, /fpga-axi@0/axi-adxcvr-rx@84a60000 <-> /fpga-axi@0/axi-jesd204-rx@84aa0000
[    0.667908] jesd204: created con: id=4, topo=0, link=0, /fpga-axi@0/axi-jesd204-tx@84a90000 <-> /fpga-axi@0/axi-adrv904x-tx-hpc@84a04000
[    0.667938] jesd204: created con: id=5, topo=0, link=2, /fpga-axi@0/axi-jesd204-rx@84aa0000 <-> /axi/spi@ff040000/adrv904x-phy@0
[    0.667967] jesd204: created con: id=6, topo=0, link=0, /fpga-axi@0/axi-adrv904x-tx-hpc@84a04000 <-> /axi/spi@ff040000/adrv904x-phy@0
[    0.668003] jesd204: /axi/spi@ff040000/adrv904x-phy@0: JESD204[0:0] transition uninitialized -> initialized
[    0.668025] jesd204: /axi/spi@ff040000/adrv904x-phy@0: JESD204[0:2] transition uninitialized -> initialized
[    0.668047] jesd204: found 7 devices and 1 topologies
[    0.668092] FPGA manager framework
[    0.668135] Advanced Linux Sound Architecture Driver Initialized.
[    0.668731] Bluetooth: Core ver 2.22
[    0.668759] NET: Registered PF_BLUETOOTH protocol family
[    0.668769] Bluetooth: HCI device and connection manager initialized
[    0.668782] Bluetooth: HCI socket layer initialized
[    0.668793] Bluetooth: L2CAP socket layer initialized
[    0.668809] Bluetooth: SCO socket layer initialized
[    0.669223] vgaarb: loaded
[    0.669443] clocksource: Switched to clocksource arch_sys_counter
[    0.669584] VFS: Disk quotas dquot_6.6.0
[    0.669615] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.674801] NET: Registered PF_INET protocol family
[    0.674964] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.677690] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[    0.677735] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.677754] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.677972] TCP bind hash table entries: 32768 (order: 8, 1048576 bytes, linear)
[    0.678816] TCP: Hash tables configured (established 32768 bind 32768)
[    0.678895] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.678977] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.679127] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.679538] RPC: Registered named UNIX socket transport module.
[    0.679550] RPC: Registered udp transport module.
[    0.679559] RPC: Registered tcp transport module.
[    0.679567] RPC: Registered tcp-with-tls transport module.
[    0.679575] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.680535] PCI: CLS 0 bytes, default 64
[    0.681505] Initialise system trusted keyrings
[    0.681612] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[    0.682059] NFS: Registering the id_resolver key type
[    0.682083] Key type id_resolver registered
[    0.682093] Key type id_legacy registered
[    0.682113] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.682125] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.682148] jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
[    0.682220] fuse: init (API version 7.39)
[    0.715429] NET: Registered PF_ALG protocol family
[    0.715445] xor: measuring software checksum speed
[    0.719358]    8regs           :  2523 MB/sec
[    0.723270]    32regs          :  2523 MB/sec
[    0.727455]    arm64_neon      :  2359 MB/sec
[    0.727464] xor: using function: 32regs (2523 MB/sec)
[    0.727476] Key type asymmetric registered
[    0.727487] Asymmetric key parser 'x509' registered
[    0.727523] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[    0.727537] io scheduler mq-deadline registered
[    0.727546] io scheduler kyber registered
[    0.727567] io scheduler bfq registered
[    0.764195] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    0.771466] brd: module loaded
[    0.774912] loop: module loaded
[    0.775550] Registered mathworks_ip class
[    0.776119] mtdoops: mtd device (mtddev=name/number) must be supplied
[    0.779371] tun: Universal TUN/TAP device driver, 1.6
[    0.779500] CAN device driver interface
[    0.780313] SPI driver wl1271_spi has no spi_device_id for ti,wl1271
[    0.780325] SPI driver wl1271_spi has no spi_device_id for ti,wl1273
[    0.780335] SPI driver wl1271_spi has no spi_device_id for ti,wl1281
[    0.780344] SPI driver wl1271_spi has no spi_device_id for ti,wl1283
[    0.780353] SPI driver wl1271_spi has no spi_device_id for ti,wl1285
[    0.780362] SPI driver wl1271_spi has no spi_device_id for ti,wl1801
[    0.780371] SPI driver wl1271_spi has no spi_device_id for ti,wl1805
[    0.780380] SPI driver wl1271_spi has no spi_device_id for ti,wl1807
[    0.780389] SPI driver wl1271_spi has no spi_device_id for ti,wl1831
[    0.780398] SPI driver wl1271_spi has no spi_device_id for ti,wl1835
[    0.780407] SPI driver wl1271_spi has no spi_device_id for ti,wl1837
[    0.780521] usbcore: registered new interface driver asix
[    0.780552] usbcore: registered new interface driver ax88179_178a
[    0.780579] usbcore: registered new interface driver cdc_ether
[    0.780608] usbcore: registered new interface driver net1080
[    0.780635] usbcore: registered new interface driver cdc_subset
[    0.780662] usbcore: registered new interface driver zaurus
[    0.780698] usbcore: registered new interface driver cdc_ncm
[    0.780725] usbcore: registered new interface driver r8153_ecm
[    0.781948] usbcore: registered new interface driver uas
[    0.781979] usbcore: registered new interface driver usb-storage
[    0.782042] usbcore: registered new interface driver usbserial_generic
[    0.782067] usbserial: USB Serial support registered for generic
[    0.782092] usbcore: registered new interface driver ftdi_sio
[    0.782115] usbserial: USB Serial support registered for FTDI USB Serial Device
[    0.782142] usbcore: registered new interface driver upd78f0730
[    0.782165] usbserial: USB Serial support registered for upd78f0730
[    0.783260] SPI driver ads7846 has no spi_device_id for ti,tsc2046
[    0.783272] SPI driver ads7846 has no spi_device_id for ti,ads7843
[    0.783282] SPI driver ads7846 has no spi_device_id for ti,ads7845
[    0.783291] SPI driver ads7846 has no spi_device_id for ti,ads7873
[    0.783906] rtc_zynqmp ffa60000.rtc: registered as rtc0
[    0.783930] rtc_zynqmp ffa60000.rtc: setting system clock to 2023-08-02T08:05:39 UTC (1690963539)
[    0.784010] i2c_dev: i2c /dev entries driver
[    0.784629] usbcore: registered new interface driver uvcvideo
[    0.786421] Bluetooth: HCI UART driver ver 2.3
[    0.786433] Bluetooth: HCI UART protocol H4 registered
[    0.786442] Bluetooth: HCI UART protocol BCSP registered
[    0.786467] Bluetooth: HCI UART protocol LL registered
[    0.786477] Bluetooth: HCI UART protocol ATH3K registered
[    0.786499] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    0.786544] Bluetooth: HCI UART protocol Intel registered
[    0.786567] Bluetooth: HCI UART protocol QCA registered
[    0.786598] usbcore: registered new interface driver bcm203x
[    0.786626] usbcore: registered new interface driver bpa10x
[    0.786653] usbcore: registered new interface driver bfusb
[    0.786680] usbcore: registered new interface driver btusb
[    0.786721] usbcore: registered new interface driver ath3k
[    0.786816] EDAC MC: ECC not enabled
[    0.787173] sdhci: Secure Digital Host Controller Interface driver
[    0.787184] sdhci: Copyright(c) Pierre Ossman
[    0.787192] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.787684] ledtrig-cpu: registered to indicate activity on CPUs
[    0.787749] SMCCC: SOC_ID: ID = jep106:0049:0000 Revision = 0x24738093
[    0.787830] zynqmp_firmware_probe Platform Management API v1.1
[    0.787887] zynqmp_firmware_probe Trustzone version v1.0
[    0.815780] zynqmp-aes zynqmp-aes.0: will run requests pump with realtime priority
[    0.816342] usbcore: registered new interface driver usbhid
[    0.816355] usbhid: USB HID core driver
[    0.816512] SPI driver fb_seps525 has no spi_device_id for syncoam,seps525
[    0.824323] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    0.824892] axi_sysid 85000000.axi-sysid-0: AXI System ID core version (1.01.a) found
[    0.825256] axi_sysid 85000000.axi-sysid-0: [adrv904x] on [zcu102] git branch <> git <0> dirty [2025-12-16 13:55:50] UTC
[    0.826106] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    0.826487] usbcore: registered new interface driver snd-usb-audio
[    0.828319] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    0.828778] Initializing XFRM netlink socket
[    0.828842] NET: Registered PF_INET6 protocol family
[    0.829393] Segment Routing with IPv6
[    0.829451] In-situ OAM (IOAM) with IPv6
[    0.829515] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    0.829882] NET: Registered PF_PACKET protocol family
[    0.829900] NET: Registered PF_KEY protocol family
[    0.830006] can: controller area network core
[    0.830043] NET: Registered PF_CAN protocol family
[    0.830054] can: raw protocol
[    0.830064] can: broadcast manager protocol
[    0.830077] can: netlink gateway - max_hops=1
[    0.830157] Bluetooth: RFCOMM TTY layer initialized
[    0.830176] Bluetooth: RFCOMM socket layer initialized
[    0.830198] Bluetooth: RFCOMM ver 1.11
[    0.830212] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    0.830221] Bluetooth: BNEP filters: protocol multicast
[    0.830233] Bluetooth: BNEP socket layer initialized
[    0.830242] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    0.830253] Bluetooth: HIDP socket layer initialized
[    0.830438] 9pnet: Installing 9P2000 support
[    0.830459] NET: Registered PF_IEEE802154 protocol family
[    0.830494] Key type dns_resolver registered
[    0.837694] registered taskstats version 1
[    0.837707] Loading compiled-in X.509 certificates
[    0.843364] Btrfs loaded, zoned=no, fsverity=no
[    0.843545] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
[    1.260485] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 22, base_baud = 6249999) is a xuartps
[    1.260545] printk: console [ttyPS0] enabled
[    2.919530] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 23, base_baud = 6249999) is a xuartps
[    2.930080] nwl-pcie fd0e0000.pcie: host bridge /axi/pcie@fd0e0000 ranges:
[    2.936996] nwl-pcie fd0e0000.pcie:      MEM 0x00e0000000..0x00efffffff -> 0x00e0000000
[    2.945020] nwl-pcie fd0e0000.pcie:      MEM 0x0600000000..0x07ffffffff -> 0x0600000000
[    2.953135] nwl-pcie fd0e0000.pcie: Link is DOWN
[    2.958221] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
[    2.964409] pci_bus 0000:00: root bus resource [bus 00-ff]
[    2.969904] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
[    2.976781] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
[    2.984288] pci 0000:00:00.0: [10ee:d021] type 01 class 0x060400
[    2.990355] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[    2.998449] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    3.006586] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[    3.013213] pci 0000:00:00.0: PCI bridge to [bus 01]
[    3.021540] ad9528 spi1.1: supply vcc not found, using dummy regulator
[    3.063169] jesd204: /axi/spi@ff040000/ad9528-1@1,jesd204:0,parent=spi1.1: Using as SYSREF provider
[    3.073148] MESSAGE: API_LOG:-> adi_adrv904x_HwOpen()
[    3.078207] MESSAGE: API_LOG:adi_adrv904x_HwOpen(...)
[    3.083260] MESSAGE: API_LOG:-> adi_adrv904x_HwReset()
[    3.138480] MESSAGE: API_LOG:-> adi_adrv904x_SpiCfgSet()
[    3.143986] MESSAGE: API_LOG:-> adi_adrv904x_GpioDriveStrengthSet()
[    3.150486] MESSAGE: API_LOG:<- adi_adrv904x_GpioDriveStrengthSet()
[    3.156756] MESSAGE: API_LOG:-> adi_adrv904x_GpioDriveStrengthSet()
[    3.163131] MESSAGE: API_LOG:<- adi_adrv904x_GpioDriveStrengthSet()
[    3.169402] MESSAGE: API_LOG:-> adi_adrv904x_GpioHysteresisSet()
[    3.175465] MESSAGE: API_LOG:<- adi_adrv904x_GpioHysteresisSet()
[    3.181476] MESSAGE: API_LOG:<- adi_adrv904x_SpiCfgSet()
[    3.186785] MESSAGE: API_LOG:<- adi_adrv904x_HwReset()
[    3.191922] MESSAGE: API_LOG:<- adi_adrv904x_HwOpen()
[    3.196975] MESSAGE: API_LOG:-> adi_adrv904x_SpiVerify()
[    3.202456] MESSAGE: API_LOG:<- adi_adrv904x_SpiVerify()
[    3.207767] MESSAGE: API_LOG:-> adi_adrv904x_ApiVersionGet()
[    3.213424] MESSAGE: API_LOG:<- adi_adrv904x_ApiVersionGet()
[    3.219086] adrv9040 spi1.0: adrv9040 Rev 0, API version: 2.10.0.4 found
[    3.225793] MESSAGE: API_LOG:-> adi_adrv904x_InitDataExtract()
[    3.231671] MESSAGE: API_LOG:<- adi_adrv904x_InitDataExtract()
[    3.237502]
[    3.237502]  Using the Profile Init and PostMcsInit Structures
[    3.244814] MESSAGE: API_LOG:-> adi_adrv904x_DeviceInfoExtract()
[    3.250859] MESSAGE: API_LOG:<- adi_adrv904x_DeviceInfoExtract()
[    3.257039] MESSAGE: API_LOG:adrv904x_TxLinkSamplingRateFind(...)
[    3.264265] MESSAGE: API_LOG:-> adi_adrv904x_ApiVersionGet()
[    3.269926] MESSAGE: API_LOG:<- adi_adrv904x_ApiVersionGet()
[    3.275582] MESSAGE: API_LOG:-> adi_adrv904x_HwClose()
[    3.280720] MESSAGE: API_LOG:<- adi_adrv904x_HwClose()
[    3.285859] adrv9040 spi1.0: adrv9040 Rev 0, API version: 2.10.0.4 found
[    3.293357] spi-nor spi0.0: SPI-NOR-UniqueID b2e30100140f000a00ed42a01e28
[    3.300154] spi-nor spi0.0: found mt25qu512a, expected m25p80
[    3.306168] spi-nor spi0.0: mt25qu512a (131072 Kbytes)
[    3.311410] 4 fixed-partitions partitions found on MTD device spi0.0
[    3.317770] Creating 4 MTD partitions on "spi0.0":
[    3.322556] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[    3.329199] 0x000000100000-0x000000600000 : "qspi-linux"
[    3.335270] 0x000000600000-0x000000620000 : "qspi-device-tree"
[    3.341854] 0x000000620000-0x000000c00000 : "qspi-rootfs"
[    3.374449] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    3.381049] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[    3.387554] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[    3.394059] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[    3.401359] i2c i2c-0: using pinctrl states for GPIO recovery
[    3.407305] i2c i2c-0: using generic GPIOs for recovery
[    3.412946] pca953x 0-0020: supply vcc not found, using dummy regulator
[    3.419650] pca953x 0-0020: using no AI
[    3.425147] pca953x 0-0021: supply vcc not found, using dummy regulator
[    3.431831] pca953x 0-0021: using no AI
[    3.436499] pca954x 0-0075: supply vdd not found, using dummy regulator
[    3.443654] ina2xx 2-0040: supply vs not found, using dummy regulator
[    3.450574] ina2xx 2-0040: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.457121] ina2xx 2-0041: supply vs not found, using dummy regulator
[    3.463957] ina2xx 2-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.470507] ina2xx 2-0042: supply vs not found, using dummy regulator
[    3.477361] ina2xx 2-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.483913] ina2xx 2-0043: supply vs not found, using dummy regulator
[    3.490751] ina2xx 2-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.497293] ina2xx 2-0044: supply vs not found, using dummy regulator
[    3.504136] ina2xx 2-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.510689] ina2xx 2-0045: supply vs not found, using dummy regulator
[    3.517528] ina2xx 2-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.524068] ina2xx 2-0046: supply vs not found, using dummy regulator
[    3.530911] ina2xx 2-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.537464] ina2xx 2-0047: supply vs not found, using dummy regulator
[    3.544312] ina2xx 2-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.550858] ina2xx 2-004a: supply vs not found, using dummy regulator
[    3.557696] ina2xx 2-004a: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.564245] ina2xx 2-004b: supply vs not found, using dummy regulator
[    3.571076] ina2xx 2-004b: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.577501] i2c i2c-0: Added multiplexed i2c bus 2
[    3.582635] ina2xx 3-0040: supply vs not found, using dummy regulator
[    3.589561] ina2xx 3-0040: power monitor ina226 (Rshunt = 2000 uOhm)
[    3.596106] ina2xx 3-0041: supply vs not found, using dummy regulator
[    3.602941] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.609490] ina2xx 3-0042: supply vs not found, using dummy regulator
[    3.616327] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.622893] ina2xx 3-0043: supply vs not found, using dummy regulator
[    3.629744] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.636283] ina2xx 3-0044: supply vs not found, using dummy regulator
[    3.643123] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.649671] ina2xx 3-0045: supply vs not found, using dummy regulator
[    3.656510] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.663066] ina2xx 3-0046: supply vs not found, using dummy regulator
[    3.669904] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.676448] ina2xx 3-0047: supply vs not found, using dummy regulator
[    3.683289] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.689705] i2c i2c-0: Added multiplexed i2c bus 3
[    3.740384] i2c i2c-0: Added multiplexed i2c bus 4
[    3.745371] i2c i2c-0: Added multiplexed i2c bus 5
[    3.750167] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
[    3.757559] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 46
[    3.764596] i2c i2c-1: using pinctrl states for GPIO recovery
[    3.770544] i2c i2c-1: using generic GPIOs for recovery
[    3.776189] pca954x 1-0074: supply vdd not found, using dummy regulator
[    3.783277] at24 6-0054: supply vcc not found, using dummy regulator
[    3.790175] at24 6-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
[    3.796941] i2c i2c-1: Added multiplexed i2c bus 6
[    3.802349] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.809670] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.816982] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.824294] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.831608] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.838916] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.846231] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.853553] si5341 7-0036: no regulator set, defaulting vdd_sel to 2.5V for out
[    3.861629] si5341 7-0036: Chip: 5341 Grade: 1 Rev: 1
[    3.889359] i2c i2c-1: Added multiplexed i2c bus 7
[    3.896389] si570 8-005d: registered, current frequency 300000000 Hz
[    3.902808] i2c i2c-1: Added multiplexed i2c bus 8
[    3.909804] si570 9-005d: registered, current frequency 156250000 Hz
[    3.916218] i2c i2c-1: Added multiplexed i2c bus 9
[    3.921277] si5324 10-0069: si5328 probed
[    3.987081] si5324 10-0069: si5328 probe successful
[    3.992024] i2c i2c-1: Added multiplexed i2c bus 10
[    3.997097] i2c i2c-1: Added multiplexed i2c bus 11
[    4.002161] i2c i2c-1: Added multiplexed i2c bus 12
[    4.007232] i2c i2c-1: Added multiplexed i2c bus 13
[    4.012121] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
[    4.019895] pca954x 1-0075: supply vdd not found, using dummy regulator
[    4.026873] i2c i2c-1: Added multiplexed i2c bus 14
[    4.032275] ad7291: probe of 15-002f failed with error -5
[    4.037865] at24 15-0050: supply vcc not found, using dummy regulator
[    4.072707] i2c i2c-1: Added multiplexed i2c bus 15
[    4.077796] i2c i2c-1: Added multiplexed i2c bus 16
[    4.082870] i2c i2c-1: Added multiplexed i2c bus 17
[    4.087949] i2c i2c-1: Added multiplexed i2c bus 18
[    4.093028] i2c i2c-1: Added multiplexed i2c bus 19
[    4.098113] i2c i2c-1: Added multiplexed i2c bus 20
[    4.103191] i2c i2c-1: Added multiplexed i2c bus 21
[    4.108078] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
[    4.115709] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 47
[    4.125048] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
[    4.153445] iio_dmaengine_buffer_alloc:303 width 0 (DMA width >= 256-bits ?)
[    4.161389] cf_axi_adc 84a00000.axi-adrv904x-rx-hpc: ADI AIM (10.03.) probed ADC ADRV904X as MASTER
[    4.165445] mmc0: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[    4.189465] iio_dmaengine_buffer_alloc:303 width 0 (DMA width >= 256-bits ?)
[    4.198881] cf_axi_dds 84a04000.axi-adrv904x-tx-hpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.02.b) at 0x84A04000 mapped to 0x(____ptrval____), probed DDS ADRV904X
[    4.213976] axi_adxcvr_drv 84a60000.axi-adxcvr-rx: adxcvr_enforce_settings: Using QPLL without access, assuming desired Lane rate will be configured by a different instance
[    4.230863] axi_adxcvr_drv 84a60000.axi-adxcvr-rx: AXI-ADXCVR-RX (17.05.a) using QPLL on GTH4. Number of lanes: 8.
[    4.242211] axi_adxcvr_drv 84a80000.axi-adxcvr-tx: AXI-ADXCVR-TX (17.05.a) using QPLL on GTH4. Number of lanes: 8.
[    4.253157] axi-jesd204-rx 84aa0000.axi-jesd204-rx: AXI-JESD204-RX (1.07.a). Encoder 64b66b, width 8/8, lanes 8, jesd204-fsm.
[    4.264891] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition initialized -> probed
[    4.276132] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition initialized -> probed
[    4.287373] MESSAGE: API_LOG:-> adi_adrv904x_HwOpen()
[    4.292429] MESSAGE: API_LOG:adi_adrv904x_HwOpen(...)
[    4.297478] MESSAGE: API_LOG:-> adi_adrv904x_HwReset()
[    4.305987] mmc0: new high speed SDHC card at address 5048
[    4.311860] mmcblk0: mmc0:5048 SDCHE 29.0 GiB
[    4.317821]  mmcblk0: p1 p2 p3
[    4.352710] MESSAGE: API_LOG:-> adi_adrv904x_SpiCfgSet()
[    4.358052] MESSAGE: API_LOG:-> adi_adrv904x_GpioDriveStrengthSet()
[    4.364554] MESSAGE: API_LOG:<- adi_adrv904x_GpioDriveStrengthSet()
[    4.370826] MESSAGE: API_LOG:-> adi_adrv904x_GpioDriveStrengthSet()
[    4.377203] MESSAGE: API_LOG:<- adi_adrv904x_GpioDriveStrengthSet()
[    4.383476] MESSAGE: API_LOG:-> adi_adrv904x_GpioHysteresisSet()
[    4.389547] MESSAGE: API_LOG:<- adi_adrv904x_GpioHysteresisSet()
[    4.395555] MESSAGE: API_LOG:<- adi_adrv904x_SpiCfgSet()
[    4.400865] MESSAGE: API_LOG:<- adi_adrv904x_HwReset()
[    4.406008] MESSAGE: API_LOG:<- adi_adrv904x_HwOpen()
[    5.573471] random: crng init done
[    6.059776] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition probed -> initialized
[    6.071018] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition probed -> initialized
[    7.727856] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition initialized -> probed
[    7.739109] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition initialized -> probed
[    9.395766] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition probed -> idle
[    9.406407] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition probed -> idle
[   11.062598] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition idle -> device_init
[   11.073670] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition idle -> device_init
[   11.106048] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition device_init -> link_init
[   11.117543] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition device_init -> link_init
[   11.129045] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition link_init -> link_supported
[   11.140794] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition link_init -> link_supported
[   11.152825] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition link_supported -> link_pre_setup
[   11.165015] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition link_supported -> link_pre_setup
[   11.177447] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition link_pre_setup -> clk_sync_stage1
[   11.189729] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition link_pre_setup -> clk_sync_stage1
[   11.202000] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition clk_sync_stage1 -> clk_sync_stage2
[   11.214357] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition clk_sync_stage1 -> clk_sync_stage2
[   11.226724] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition clk_sync_stage2 -> clk_sync_stage3
[   11.239078] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition clk_sync_stage2 -> clk_sync_stage3
[   11.256127] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition clk_sync_stage3 -> link_setup
[   11.268054] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition clk_sync_stage3 -> link_setup
[   11.280652] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:0] transition link_setup -> opt_setup_stage1
[   11.292671] jesd204: /axi/spi@ff040000/adrv904x-phy@0,jesd204:1,parent=spi1.0: JESD204[0:2] transition link_setup -> opt_setup_stage1
[   11.665495] Insufficient stack space to handle exception!
[   11.665499] ESR: 0x0000000096000047 -- DABT (current EL)
[   11.665503] FAR: 0xffffffc082beffd0
[   11.665505] Task stack:     [0xffffffc082bf0000..0xffffffc082bf4000]
[   11.665509] IRQ stack:      [0xffffffc080000000..0xffffffc080004000]
[   11.665512] Overflow stack: [0xffffff887f7622d0..0xffffff887f7632d0]
[   11.665516] CPU: 0 PID: 38 Comm: kworker/u9:1 Not tainted 6.6.0 #1
[   11.665523] Hardware name: ZynqMP ZCU102 Rev1.0 (DT)
[   11.665528] Workqueue: events_unbound deferred_probe_work_func
[   11.665544] pstate: 200000c5 (nzCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   11.665551] pc : update_group_capacity+0x4/0x1dc
[   11.665560] lr : update_sd_lb_stats.constprop.0+0xd4/0x84c
[   11.665568] sp : ffffffc082bf0000
[   11.665570] x29: ffffffc082bf0000 x28: ffffffc0827e8c28 x27: ffffffc082bf02c0
[   11.665579] x26: ffffff8800082300 x25: 0000000000000000 x24: ffffffc082bf0118
[   11.665588] x23: ffffffc082571980 x22: ffffffc082bf0318 x21: ffffff8800082300
[   11.665597] x20: ffffffc08256b9d0 x19: ffffffc082bf0098 x18: 0000000000000006
[   11.665605] x17: 2e316970733d746e x16: 657261702c313a34 x15: 0000000000000000
[   11.665613] x14: 008587642f05b66a x13: 0085a58b28fc938a x12: 0000000000000002
[   11.665621] x11: 0000000000000048 x10: 0000000000000051 x9 : 0000000000000000
[   11.665628] x8 : ffffffc082bf00e8 x7 : 0000000000000000 x6 : 000000000000003f
[   11.665636] x5 : 0000000000000040 x4 : 0000000000000008 x3 : 0000000000000000
[   11.665644] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffffff8800180900
[   11.665653] Kernel panic - not syncing: kernel stack overflow
[   11.665656] CPU: 0 PID: 38 Comm: kworker/u9:1 Not tainted 6.6.0 #1
[   11.665662] Hardware name: ZynqMP ZCU102 Rev1.0 (DT)
[   11.665664] Workqueue: events_unbound deferred_probe_work_func
[   11.665674] Call trace:
[   11.665676]  dump_backtrace+0x94/0xec
[   11.665686]  show_stack+0x18/0x24
[   11.665694]  dump_stack_lvl+0x48/0x60
[   11.665702]  dump_stack+0x18/0x24
[   11.665708]  panic+0x2fc/0x350
[   11.665714]  nmi_panic+0x8c/0x90
[   11.665719]  panic_bad_stack+0xe4/0xf0
[   11.665725]  handle_bad_stack+0x34/0xbc
[   11.665733]  __bad_stack+0x78/0x7c
[   11.665738]  update_group_capacity+0x4/0x1dc
[   11.665745]  find_busiest_group+0x48/0x448
[   11.665752]  load_balance+0x240/0x9b8
[   11.665759]  newidle_balance.constprop.0+0x174/0x3e8
[   11.665767]  pick_next_task_fair+0x40/0x354
[   11.665774]  __schedule+0x118/0x7e4
[   11.665782]  schedule+0x50/0xac
[   11.665789]  schedule_timeout+0x8c/0x100
[   11.665795]  __wait_for_common+0xd4/0x230
[   11.665803]  wait_for_completion_timeout+0x20/0x2c
[   11.665811]  spi_transfer_one_message+0x488/0x540
[   11.665818]  __spi_pump_transfer_message+0x190/0x4a8
[   11.665824]  __spi_sync+0x208/0x2d4
[   11.665829]  spi_sync+0x30/0x54
[   11.665834]  spi_sync_transfer.constprop.0+0x78/0xa8
[   11.665845]  linux_adrv904x_SpiRead+0xc4/0x110
[   11.665854]  adrv904x_FlushParse+0x90/0x4b4
[   11.665861]  adi_adrv904x_RegistersByteRead+0x17c/0xdf0
[   11.665868]  adrv904x_CpuMailboxBufferRead+0xb4/0x3b4
[   11.665878]  adrv904x_CpuCmdRespRead+0x120/0xce0
[   11.665886]  adrv904x_CpuCmdSend+0xfc/0x71c
[   11.665894]  adi_adrv904x_InitCalsCheckCompleteGet_v2+0xa0/0x4ac
[   11.665902]  adi_adrv904x_InitCalsWait_v2+0xa8/0x3a4
[   11.665909]  adi_adrv904x_PostMcsInit+0x3e0/0xb24
[   11.665918]  adrv904x_jesd204_setup_stage2+0x70/0xf4
[   11.665924]  jesd204_fsm_table_entry_cb+0x9c/0x138
[   11.665932]  jesd204_fsm_handle_con_cb+0x88/0x2a4
[   11.665938]  __jesd204_fsm+0x3c4/0x5b0
[   11.665943]  jesd204_fsm_table+0x128/0x41c
[   11.665949]  jesd204_fsm_probe_done+0x2c/0x38
[   11.665955]  __jesd204_all_links_fsm_done_cb+0x48/0x114
[   11.665961]  __jesd204_fsm+0x454/0x5b0
[   11.665967]  __jesd204_fsm_start+0xe0/0x124
[   11.665973]  devm_jesd204_fsm_start+0x2c/0xb8
[   11.665979]  axi_jesd204_tx_probe+0x478/0x7b0
[   11.665987]  platform_probe+0x68/0xc4
[   11.665993]  really_probe+0x148/0x2ac
[   11.666001]  __driver_probe_device+0x78/0x12c
[   11.666009]  driver_probe_device+0xd8/0x15c
[   11.666016]  __device_attach_driver+0xb8/0x134
[   11.666024]  bus_for_each_drv+0x84/0xe0
[   11.666032]  __device_attach+0x9c/0x188
[   11.666039]  device_initial_probe+0x14/0x20
[   11.666048]  bus_probe_device+0xac/0xb0
[   11.666055]  deferred_probe_work_func+0x88/0xc0
[   11.666063]  process_one_work+0x138/0x28c
[   11.666070]  worker_thread+0x29c/0x4b8
[   11.666075]  kthread+0xe4/0xe8
[   11.666084]  ret_from_fork+0x10/0x20
[   11.666091] SMP: stopping secondary CPUs
[   11.666097] Kernel Offset: disabled
[   11.666099] CPU features: 0x0,00000008,00020000,0000420b
[   11.666103] Memory Limit: none
[   12.087525] ---[ end Kernel panic - not syncing: kernel stack overflow ]---

Thread Notes