Post Go back to editing

Creating custom profile

Category: Software
Product Number: ADRV9026
Software Version: API: 7.0.0.14 Firmware 7.0.0.11 Stream: 9.4.0.1 RadioVerse: 7.0.0.15

Hi, 

I would like to create a profile that keeps the same L, K, M, F, Np parameters (use the same FPGA firmware)

The parameters should be:

Rx/Tx BW: 60MHz

SRate: 245.76 MS/s

No link sharing

Tried to change that using Adrv9025 Transceiver Evaluation software, but it dosn't let me save the changes.

I took profile 51_nonLinkSharing as reference, changed the Rx/Tx RF BW.

If I save it using the "Save" button I am getting an empty profile.

Is it possible at all?

BR

Yishay

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.