Post Go back to editing

RF path/sample delay

Thread Summary

The user observed a 1ns delay in RX2 and RX3 compared to RX1 and RX4 on the ADRV9026 with a 61.44 MSPS RX sample rate and 1.966 GHz ADC sample rate. The delay is consistent and likely due to internal ADC clock cycle differences. The user will compensate for this delay in the digital domain, as no internal setting or calibration can resolve it.
AI Generated Content
Category: Hardware
Product Number: ADRV9026

We use the ADRV9026 with a 61.44 MSPS RX sample rate. The ADC sample rate is 1.966 GHz. Hardware is ZCU102+ADRV9026 evaluation board.

We need the RF path delays to be as equal as possible for all inputs. We created a tool to measure the (relative) delays. In our test, we apply a test signal to every input, using a 4-way splitter and matched cables. The splitter and cables are checked with a VNA, the delays are the same within 10's of picoseconds. 

When examining the test signal using our calibration software, we see that RX2 and RX3 are always delayed by ~ 1ns with respect to RX1 and RX4. For example, measured delays are  0.0069,  1.0002, 1.0469, 0.0000 for inputs RX1, 2, 3 and 4 (all delays with respect to the shortest one).

This is unexpected. A theory is that the delays are, for some reason, 2 ADC clock cycles delayed for RX2 and RX3? Trace delays alone are not in the 1ns range.

The profile is derived from profile 51-Non-Link-sharing. I tried to enable some additional delays but with no improvement.

Any idea why this is, and if we can improve this?

Parents Reply
  • Ok, thanks, that's what we observed. It's always the same, RX1 and RX4 are close, RX2 and RX3 are close, and there's approx. +1ns for RX2 and RX3 with respect to RX1 and RX4. 

    I had the hope that there's some internal setting/calibration to get rid of this additional nanosecond, but for now we'll compensate for it in the digital domain.

Children
No Data