Post Go back to editing

ADRV9029 Bring Up

Category: Hardware
Product Number: ADRV9029

I have a custom CCA using the ADRV9029.

I am trying to power it up, and noticing no difference in current draw, between having the RESET pin pulled low (in reset), vs pulling it up/out of reset.


I have reviewed the power supply sequencing, and currently have all 1.0 Rails Tied together, and powered up, followed by 1.3V, then 1.8V.

After reviewing the datasheet and Users Guide, I question if this is okay to have all 1.0v Rails tied together

Also have verified we are not in a Test Mode, as this is pulled down to ground.


I am curious on the most essential items to have, to be able to bring the device out of reset, and do a simple read/write over SPI.


Thanks!