Post Go back to editing

adrv9026 no-os prject:How to automatically update xparameters.h

Thread Summary

The user is trying to update the AXI base address in the xparameters.h file for a Zynq-based project using the Xilinx JESD204C IP core with the ADI No-OS framework. The final answer suggests running 'make reset' before 'make' to refresh the xparameters.h file. Additional clarification notes that xparameters.h is generated from the XSA and requires a rebuild and re-copy of the XSA if the hardware configuration changes.
AI Generated Content
Category: Software
Product Number: ADRV9026
Software Version: vitis2025.1

i want to using zynq  to config xilinx jesd204c ip core through axi lite bus. after generate my xsa file and imported to no-os. after builed i found the axi base address not reflash on the xparameters.h.

How to automatically update adrv9026 no-os projest's xparameters.h?

Thread Notes

Parents
  • Hi!

    The xparameters.h is generated from the XSA and doesn’t update automatically when the hardware changes.

    If you modified the AXI base address in Vivado, you need to rebuild and re-copy the XSA into the no-OS project. After that, xparameters.h will be regenerated with the correct addresses.

    Regards, Elena

Reply
  • Hi!

    The xparameters.h is generated from the XSA and doesn’t update automatically when the hardware changes.

    If you modified the AXI base address in Vivado, you need to rebuild and re-copy the XSA into the no-OS project. After that, xparameters.h will be regenerated with the correct addresses.

    Regards, Elena

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.