ADRV9029
Recommended for New Designs
The ADRV9029 is a highly integrated, radio frequency (RF) agile transceiver offering four independently controlled transmitters, dedicated observation...
Datasheet
ADRV9029 on Analog.com

Sorry to have missed this. What is the reference clock that you are using? What is your test setup? Which profile are you using- Default or custom one?
Sorry to have missed this. What is the reference clock that you are using? What is your test setup? Which profile are you using- Default or custom one?
We are using dev clock of 122.88 MHz and sysref of 60 kHz and a custom profile which I have attached. Thanks
{
"radioCtrlInit": {
"radioCtrlModeCfg": {
"txRadioCtrlModeCfg": {
"txEnableMode": 0,
"txChannelMask": 15
},
"rxRadioCtrlModeCfg": {
"rxEnableMode": 0,
"rxChannelMask": 255
},
"orxRadioCtrlModeCfg": {
"orxEnableMode": 0,
"orxPinSelectSettlingDelay_armClkCycles": 0,
"singleChannel1PinModeOrxSel": 0,
"singleChannel2PinModeLowOrxSel": 0,
"singleChannel2PinModeHighOrxSel": 0,
"dualChannel2PinModeOrxSel": 0
}
},
"txToOrxMapping": {
"orx1Map": 2,
"orx2Map": 3,
"orx3Map": 2,
"orx4Map": 3
},
"streamGpioCfg": {
"streamGpInput0": 19,
"streamGpInput1": 19,
"streamGpInput2": 19,
"streamGpInput3": 19,
"streamGpInput4": 19,
"streamGpInput5": 19,
"streamGpInput6": 19,
"streamGpInput7": 19,
"streamGpInput8": 19,
"streamGpInput9": 19,
"streamGpInput10": 19,
"streamGpInput11": 19,
"streamGpInput12": 19,
"streamGpInput13": 19,
"streamGpInput14": 19,
"streamGpInput15": 19
},
"lo1PllFreq_Hz": 3500000000,
"lo2PllFreq_Hz": 3550000000,
"auxPllFreq_Hz": 0
},
"initCals": {
"calMask": 862207,
"channelMask": 15,
"warmBoot": 0
},
"calRsltsFile": null,
"checkFwVer": 0
}