Post Go back to editing

ADRV9029 on ZCU102: CPU stuck in Powerup mode (Error 0x12020000) during BoardProgram

Category: Software
Product Number: ADRV9029

Hi ADI Team,

I am porting the ADRV9029 SDK example to a ZCU102 platform. While I have successfully locked the AD9528 PLL2, I am hitting a critical failure during the BoardProgram phase (Step 7).

Issue Summary: The initialization fails with error 0x12020000 at adi_adrv9025_CpuStartStatusCheck. The CPU status registers consistently return 0x00.

Key Log Snippets:

Plaintext
[1] Chip ID Check: 0x00
[2] Power Status (Reg 0x0018): 0x00
[3] ARM System Status (Reg 0x0080): 0x00
[4] ARM Boot Status (Reg 0x0081): 0x00
...
Error message CpuBootStatus_e: 1 - : CPU is stuck in Powerup mode. === ENTERING MAIN ===Step 0: Power Up & Reset (Moved to StaPlatform: Enabling Level Shifters & PVT Power...
HAL_DEBUG: Sysfs GPIO 458 -> 1 OK
Platform: Enabling MGT Power (GPIO 303/304)...
HAL_DEBUG: Sysfs GPIO 303 -> 1 OK
HAL_DEBUG: Sysfs GPIO 304 -> 1 OK
HAL_DEBUG: Sysfs GPIO 470 -> 0 OK
Platform: Performing Hardware Reset (GPIO 480) for AD9528...
HAL_DEBUG: Direct GPIO Write (Pin 480 -> 0, Bank 5, Bit 4) Done.
HAL_DEBUG: Direct GPIO Write (Pin 480 -> 1, Bank 5, Bit 4) Done.
Platform: Performing Hardware Reset (GPIO 469 & 506) for ADRV9025...
HAL_DEBUG: Sysfs GPIO 469 -> 0 OK
HAL_DEBUG: Direct GPIO Write (Pin 506 -> 0, Bank 5, Bit 30) Done.
HAL_DEBUG: Sysfs GPIO 469 -> 1 OK
HAL_DEBUG: Direct GPIO Write (Pin 506 -> 1, Bank 5, Bit 30) Done.
Platform: Waiting 500ms for Boot...
Step 1: Motherboard Discover
INFO: SPI clock frequency successfully set to 5MHz (per User/Kernel requirement).
Step 2: GPIO Enable
Step 2: GPIO Enable
INFO: Skipping Sysfs Clock Check (Driver Unbound). Will configure AD9528 via SPI in Step 6.
Step 3: Daughterboard Discover
Didn't read the entire EEPROM input file /sys/bus/i2c/devices/6-0054/eeprom, it's too long
FRU Version number mismatch 0x38 should be 0x01
WARNING: EEPROM read failed. Forcing ZCU102 Bypass for ADRV9025...
INFO: [Motherboard] Performing Early AD9528 Clock Config...
DEBUG: Ad9528Config Inputs: Dev=245760, VCXO=122880, RefA=30720, FPGA=245760
DEBUG: Config updated for 30.72MHz RefA Input
DEBUG: Config Settings: RefAMode=3 (DIFFERENTIAL), VCXOMode=3 (DIFFERENTIAL)
DEBUG: PLL1 Settings: nDividerPll1=4, re fA_Divider=1
DEBUG: Ad9528Config Success. Using LVDS/Differential mode per device tree.
[HAL] Opening SPI Bus 1 (Fixed Mapping)...
[HAL] Target: /dev/spidev1.1 (CS 1)
[HAL] Skipping Hal-Level Probe (Expect 0x00 due to inactive Clock)...
[HAL] Opening SPI Bus 1 (Fixed Mapping)...
[HAL] Target: /dev/spidev1.0 (CS 0)
[HAL] Skipping Hal-Level Probe (Expect 0x00 due to inactive Clock)...
[HwReset] Performing Hardware Reset (GPIO 469) Count=1...
HAL_DEBUG: Writing GPIO 469 (RESETB) to 0
HAL_DEBUG: Sysfs GPIO 469 -> 0 OK
HAL_DEBUG: Writing GPIO 469 (RESETB) to 1
HAL_DEBUG: Sysfs GPIO 469 -> 1 OK
HAL_DEBUG: Post-Reset Blind Write: Enabling ADRV9025 4-Wire Mode (Reg 0x000 -> 0x18)...
HAL_DEBUG: 4-Wire Mode Enable Sent (3x).
[HwReset] Waiting 50ms for chip boot after reset release...
Step 3 Passed
Step 4: SaveInfo calls
INFO: Rx/Tx InitChannelMask enabled (0x0F). Expecting Gain Table load.
Step 4 Passed
Step 5: Device assignments
Step 5 Passed
Step 6: Clock Configuration
Step 6: Clock Configuration (User Space Init)...
DEBUG: Ad9528Config Inputs: Dev=245760, VCXO=122880, RefA=30720, FPGA=245760
DEBUG: Config updated for 30.72MHz RefA Input
DEBUG: Config Settings: RefAMode=3 (DIFFERENTIAL), VCXOMode=3 (DIFFERENTIAL)
DEBUG: PLL1 Settings: nDividerPll1=4, re fA_Divider=1
DEBUG: Ad9528Config Success. Using LVDS/Differential mode per device tree.
Step 6: Resetting AD9528 (Driver API) ...
HAL_DEBUG: Writing GPIO 480 (RESETB) to 0
HAL_DEBUG: Direct GPIO Write (Pin 480 -> 0, Bank 5, Bit 4) Done.
HAL_DEBUG: Writing GPIO 480 (RESETB) to 1
HAL_DEBUG: Direct GPIO Write (Pin 480 -> 1, Bank 5, Bit 4) Done.
Step 6: Forcing AD9528 into 4-Wire SPI Mode (Reg 0x000 = 0x10)...
Step 6: AD9528 Chip ID (Reg 0x003) = 0x05 (Expected 0x05)
Step 6: Writing Configuration to AD9528 ...
Step 6: PLL Status Check 1/5: Reg 0x508 = 0xE6
PLL1: 0, PLL2: 1, Holdover: 1, VBAT: 1
SUCCESS: AD9528 PLL2 Locked!
Step 6: Enabling Output Channels 1 & 13 (Real Registers 0x501/0x502)....
Step 6: Divider Check (Real Read):
PLL2 N2/AB (0x201) = 0x87
VCO Div (0x204) = 0x03
Ch1 Div (0x305) = 0x04 (Val+1)
Ch13 Div (0x329) = 0x04 (Val+1)
Ch1 Mode (0x304) = 0x40 (Expected 0x40 Boost)
Step 6: Reverting AD9528 to 3-Wire SPI Mode (Freeing MISO)...
Step 6: Post-Revert ID Check (Reg 0x003) = 0x00
SUCCESS: AD9528 MISO Released.

Observation & Questions:

  1. SPI / Connectivity: Although the code attempts to set 4-wire mode (Reg 0x000 = 0x18), the Chip ID remains 0x00. Is this indicative of a failed SPI write or a missing Device Clock (DEV_CLK)?

  2. AD9528 Transition: My log shows AD9528 PLL2 Locked, but right after reverting to 3-wire mode, the ID check becomes 0x00. Could the MISO line contention be preventing the ADRV9029 from communicating?

  3. ZCU102 Specifics: Since I am bypassing the official ADS9-based EEPROM check, are there specific GPIOs or power-up sequences (like Level Shifters) on the ZCU102 that need to be held high to enable the ADRV9029 SPI interface?

  4. DPD Context: Since I aim to run DPD, is there a known-good reference project for ZCU102 + ADRV9029 that handles the clocking and SPI routing correctly?

I have attached the full console log for your reference. Any insights on why the ARM stays in Powerup mode would be helpful.

Best regards

  • [1] Chip ID Check: 0x00
    [2] Power Status (Reg 0x0018): 0x00
    [3] ARM System Status (Reg 0x0080): 0x00
    [4] ARM Boot Status (Reg 0x0081): 0x00\n[5] ARM Command Status (Reg 0x0088): 0x00\n--- 状态读取完毕 ---\n\n
    Error number 302120960 (0x12020000), Recovery action -4.In file public/src/adi_adrv9025_cpu.c, in function adi_adrv9025_CpuStartStatusCheck, in line 189, variable name device.Error message CpuBootStatus_e: 1 - : CPU is stuck in Powerup mode.
    Error number 3 (0x00000003), Recovery action -4.In file public/src/adi_adrv9025_utilities.c, in function adi_adrv9025_PreMcsInit_NonBroadCast, in line 1446, variable name ((void *)0).Error message CpuBootStatus_e: 1 - : CPU is stuck in Powerup mode.
    ERROR: adi_adrv9025Board_Dispatch:1909 has failed.
    Error number 7 (0x00000007), Recovery action -6.In file adrv9025/src/adi_adrv9025_daughter_board.c, in function adi_adrv9025Board_Dispatch, in line 1921, variable name ((void *)0).Error message ERROR-Phase1 fail: No DaughterBoard Error
    .
    TRX Phase 1 failed.
    Failed to initialize ADRV9025 Board
    ERROR: ADRV9025 Error number 3, Recovery action -4. In file public/src/adi_adrv9025_utilities.c, in function adi_adrv9025_PreMcsInit_NonBroadCast, in line 1446, variable name ((void *)0). Error message CpuBootStatus_e: 1 - : CPU is stuck in Powerup mode.

  • There can be many reasons for this issue and see below:

    • Mismatch between Binaries, API and stream file. Load both ARM binaries generated from the same SW version.
    • Clock issues.- Device clock signal integrity , level, the frequency needs to match with what is programmed in initdata.c and meet the timing requirements.
    • SPI issue : Arm loading can fail if SPI is having issues. Check if SPI is in streaming mode.
      • SPI , Try lowering SPI speed . Scratch pad register address is 0x00A , try writing and reading back 500 times and cross check.
    • HW issues, Check Rbias resistor value is correct. Check R bias voltage . (should be ~ 0.5 V), after initialization.
    • Power supply: During Arm loading it draws more current and the voltages might drop below spec. Check power supply using oscilloscope during ARM loading.

    The following links have more details:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.