Post Go back to editing

Questions about external LO of adrv9029

Thread Summary

The user is experiencing issues with RX QEC calibration on the ADRV9029 when using an external LO at 3.69 GHz, 5 dBm. The final answer confirms that the ADRV9029 does not support external LO, despite the user's profile settings indicating otherwise. The user also asks about ORX calibration and the power range for the external LO, as well as a frequency gap between TX and ORX channels.
AI Generated Content
Category: Software
Product Number: adrv9029
Software Version: 2022.2

Hi

    My hdl and linux version are version 2022.2. I want to use external LO instead of internal, so using clock source generate 3.69GHz, 5dBm clock to LO1 and LO2, the setting of profile is: 

  "clocks": {
    "deviceClock_kHz": 245760,
    "clkPllVcoFreq_kHz": 9830400,
    "serdesPllVcoFreq_kHz": 9830400,
    "ldoSelect": 0,
    "extLoFreq1_kHz": 3690000,
    "extLoFreq2_kHz": 3690000,
    "rfPll1LoMode": 2,
    "rfPll2LoMode": 2,
    "rfPll1LoOutDivider": 0,
    "rfPll2LoOutDivider": 0,
    "rfPllPhaseSyncMode": 2,
    "rx12LoSelect": 1,
    "rx34LoSelect": 1,
    "tx12LoSelect": 2,
    "tx34LoSelect": 2,
    "orx12LoSelect": 1,
    "orx34LoSelect": 1
  },

    The linux system can boot up normal and jesd works fine, but when I executing init QEC calibration calibration_rx_qec_en, it showed errors:

    But calibration_tx_qec_en and lo calibration can work. So I have 3 questions:

    1. Why rx QEC calibration can't work when using external LO

    2. Does the rx contains orx? If not, how to calibration orx channel.

    3. What is the power range of external LO, I set it to 5dBm but  tx dc too large. But less 5dBm, the jesd can't establish

    4. There exist frequency gap when tx send to orx receive, about 3.5KHz, it seems the ORX did not use the external for there should not exist frequency gap between tx and orx if orx also use external LO, does my profile wrong?

Thanks

Edit Notes

Additional questions
[edited by: mozhoudonglu at 9:31 AM (GMT -5) on 30 Jan 2026]