Post Go back to editing

ADRV9026 TX_EN behavior and TX datapath latency

Category: Datasheet/Specs
Product Number: ADRV9026

Is it appropriate to control (toggle) the TX_EN pin of the ADRV9026 during operation?

If TX_EN can be toggled, what limitations or constraints should be considered to avoid losing transmitted (TX) data?

For example:

  • Is there a minimum required off-time between two consecutive TX_EN assertions (0 → 1)?

  • When transmitting a short TX burst (e.g. 1 µs of valid TX data), what is the minimum required TX_EN high duration to ensure the data is not lost or truncated?

Any guidance on recommended timing or usage of TX_EN for short-burst or TDD-style transmission on the ADRV9026 would be appreciated.