Post Go back to editing

Receive only using ORx instead of RX

Thread Summary

The user inquired about configuring the ADRV9029 to use two ORx paths with 450 MHz bandwidth each instead of four RX paths with 200 MHz bandwidth. The final answer indicates this is not possible at their end. The ORx path is not designed for typical receiver use and lacks gain control, making it unsuitable for this application. The user planned to combine the 900 MHz bandwidth at the FPGA, but this configuration has not been tested.
AI Generated Content
Category: Software
Product Number: ADRV9029
Software Version: 6.4.0.14

Hi ADI,

In our application, there are time when we config the ADRV9029 to be a receiver only. So I want to know if we can use 2 ORx path, each one has 450MHz bandwidth, instead of 4 RX path with 200MHz bandwidth each, for receiving signals? And how to do it if it is possible?

Thank you.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.