Post Go back to editing

Generating QAM baseband I/Q file for ADRV9025 — normalization and RRC filter question

Thread Summary

The user is generating a 16-QAM baseband signal in MATLAB for use with the ADRV9025 in TES. The final answer confirms that the IQ file should be non-normalized and IQ tabbed, and the RRC filter must be applied in MATLAB. The user's transmitted spectrum appears flat, likely due to mismatched sample rates between MATLAB (983.04 MSPS) and the ADRV9025 profile (122.880 MHz). The user should upsample/interpolate the symbols to match the ADRV9025's sample rate and ensure the waveform length is 10ms. The symbol rate in the VSA should be calculated using Rs = Fs / samples per symbol, where Fs is the IQ sample rate of the Tx profile.
AI Generated Content
Category: Hardware
Product Number: ADRV9025

Hi,

I’m generating a 16-QAM baseband signal in MATLAB

I plan to export I and Q samples to a text file for use with the ADRV9025 in TES.
I have two questions:

  1. Should I normalize I/Q before exporting, or does TES handle it automatically?
     – If normalization is required, how exactly should I do it?

  2. Should I apply the RRC filter in MATLAB before export, or can I apply it directly in TES?

Thanks

Parents Reply
  • Thank you for your reply.

    The profile I am using on the ADRV9025 has a sample rate of 122.880 MHz.
    However, in my MATLAB code below, I am not specifying any sample rate. I simply generate the 16-QAM symbols and create the I/Q text file.

    How should I apply this sample rate in MATLAB when creating the I/Q file?
    Do I need to upsample/interpolate the symbols to 122.880 MHz, and if yes, what is the correct method?

    Here is the code I am using:

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.