Hello, I am using the ADRV9029. I would like to work in bare-metal mode without using Linux. I have a few questions:
1- System Boot Time in Bare-Metal Mode:
What is the boot time of the system when operating in bare-metal mode?
2- LO Switching Time:
What is the time required to switch the LO (Local Oscillator)?
3- IC Reprogramming Time:
How long does it take to reprogram the IC?
4- LO Change with TES GUI:
When using the GUI, if I change the LO, does the system automatically perform the necessary calibration after the LO change, or do I need to do this manually?
5- Calibration with External Path Using GUI:
How can I perform calibration with the external feedback path when working with the TES GUI?
Best regards.