Post Go back to editing

The question about rx noise floor of adrv9029

Category: Hardware
Product Number: ADRV9029

Hi:

The FFT spectrum of the rx IQ datas at output of adrv9029 which worked on user case 51 was shown below:

The rx data rate was 245.76MHz, sample time was 20mS, so frequency resolution was 50Hz,

The noise floor in the picture was about -120dBFs/50Hz, was -137dBFs/Hz, is that rx noise floor right?   

The rx Noise Figure on datasheet is 11.9dB at 2600MHz, how to convert the NF to rx noise floor at output of adrv9029?

Looking forward to your apply, thank you!

Parents Reply Children
  • Thanks for waiting on this.

    In the calculations, we are taking -120dBFS/50Hz as an approximate value. However, this is just one capture and within this capture as well, the noise is varying down to -130dBFS/50Hz as well if we zoom in. So, basically, we need to take multiple captures and then take average bin noise.

    In our characterization test, we do multiple captures, get a PSD from each capture, and average each individual bin across 20 captures of the same bin.

    See below, i have captured the RX samples in EVB GUI and plotted in VisualAnalog tool and its giving the expected noise floor/ noise figure.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.