Post Go back to editing

The question about rx noise floor of adrv9029

Category: Hardware
Product Number: ADRV9029

Hi:

The FFT spectrum of the rx IQ datas at output of adrv9029 which worked on user case 51 was shown below:

The rx data rate was 245.76MHz, sample time was 20mS, so frequency resolution was 50Hz,

The noise floor in the picture was about -120dBFs/50Hz, was -137dBFs/Hz, is that rx noise floor right?   

The rx Noise Figure on datasheet is 11.9dB at 2600MHz, how to convert the NF to rx noise floor at output of adrv9029?

Looking forward to your apply, thank you!

Parents Reply
  • The device worked at use case 51.  the issue is that noise floor of RX chain is higher, I want to check the noise foor of adrv9025.

    I think NF=12dB, so the noise floor at ADC input is -162dBm/Hz,  the RX chain has a gain of 18dB, so the noise floor at the output of the ADC is -144dBFs/Hz,  why is -144dBm/Hz? 

Children