Post Go back to editing

The question about rx noise floor of adrv9029

Category: Hardware
Product Number: ADRV9029

Hi:

The FFT spectrum of the rx IQ datas at output of adrv9029 which worked on user case 51 was shown below:

The rx data rate was 245.76MHz, sample time was 20mS, so frequency resolution was 50Hz,

The noise floor in the picture was about -120dBFs/50Hz, was -137dBFs/Hz, is that rx noise floor right?   

The rx Noise Figure on datasheet is 11.9dB at 2600MHz, how to convert the NF to rx noise floor at output of adrv9029?

Looking forward to your apply, thank you!

Parents Reply
  • The RX chain has a gain of 18dB at gain index of 255. In terms of dBm, the noise floor at the output of the ADC is -144dBm/Hz. The Rx full scale input power is -~12dBm which is -2dBFS. In terms of FS values, -144dBm/Hz is equivalent to -132dBFS/Hz.

    Let me know if you need any further clarifications.

    Please see this once and get back. Also, the noise figure depends on the BW, it looks like you are taking -120dBFS/Hz as the average noise floor. But if you look close to the center, the noise floor is little better.

    What is your application, are you facing any issue?

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.