Post Go back to editing

The question about rx noise floor of adrv9029

Category: Hardware
Product Number: ADRV9029

Hi:

The FFT spectrum of the rx IQ datas at output of adrv9029 which worked on user case 51 was shown below:

The rx data rate was 245.76MHz, sample time was 20mS, so frequency resolution was 50Hz,

The noise floor in the picture was about -120dBFs/50Hz, was -137dBFs/Hz, is that rx noise floor right?   

The rx Noise Figure on datasheet is 11.9dB at 2600MHz, how to convert the NF to rx noise floor at output of adrv9029?

Looking forward to your apply, thank you!

Parents Reply
  • I think the ADC conversion gain is 10dB, so the noise floor will be -174+10+12 =-152dBFs/Hz at the Rx channel ADC output.

      

    This was the spectrum when terminated the RF input port with 50Ohm, rf frequecy was 2450MHz,  BW was 245.76MHz,  gain index was 255. The rx data rate was 245.76MHz, sample time was 20mS, so frequency resolution was 50Hz,

    we can see the noise floor is -120dBFs/50Hz= -137dBFs/Hz,  the difference between theoretical noise floor(-152dBFs/Hz) is 15dB, it's abnormal.

    If this calculation process is reasonable, looking forward to your reply, thank you!

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.