Post Go back to editing

RxGain Pin Configuration

Category: Software
Product Number: ADRV9029
Software Version: 6.4.0.14

Hi,

In order to control the Rx Gain in very precise timing so i'd like to use RxGainPinControl function.

I have two question:

1. If the control and timing for all the four Rx Channel are the same, can i use only two GPIO PINs for all the four channels?

In that case, the dec pin configured for each of the four Rx channels will be same and same condition for inc pin:

    Chan0:  adi_adrv9025_GpioPinSel_erxGainIncPin = ADI_ADRV9025_GPIO_00, adi_adrv9025_GpioPinSel_erxGainDecPin = ADI_ADRV9025_GPIO_01

    Chan1:  adi_adrv9025_GpioPinSel_erxGainIncPin = ADI_ADRV9025_GPIO_00, adi_adrv9025_GpioPinSel_erxGainDecPin = ADI_ADRV9025_GPIO_01

    Chan2:  adi_adrv9025_GpioPinSel_erxGainIncPin = ADI_ADRV9025_GPIO_00, adi_adrv9025_GpioPinSel_erxGainDecPin = ADI_ADRV9025_GPIO_01

    Chan3:  adi_adrv9025_GpioPinSel_erxGainIncPin = ADI_ADRV9025_GPIO_00, adi_adrv9025_GpioPinSel_erxGainDecPin = ADI_ADRV9025_GPIO_01

while in hardware, we have GPIO_00 and 01 connected to GPIO of baseband processor.

Can we configure and connection like that?

2. Gain Step

The incStep and decStep ranges 0 to 7, so what's the exact value in dB as for the step setting?

3. Gain Inc and Dec

From the spec we can see that the gain is increased/decreased one step with a high pulse on dec/incPin. 

So does it mean we can configure the base gain in SPI mode for each Rx Channel and then switch to PIN control mode with pulses.

Then the gain change on inc/decPin will be based on the gain value we set in SPI mode?

4. Gain value sync

rxGainPinControl mode is a no-status-feedback mode for baseband. After long time of running, i guess it'd be necessary for baseband to know the real gain value that is working.

Is there any method for baseband to get the gain status under PIN control mode? or, we'd have to switch back to SPI mode to get them?

Thanks.

 

Parents
  • 1A) Ideally, 2 pins per receiver are required. I don't see any reason not to use the same GPIOs for all channels if the timing and control of the 4 channels is same. However, in real time, each receiver may be getting different signal level and the gain index may be different.

    You can try testing this in EVB and then confirm.

    2A) It depends on the gain table you use. The default gain table has 0.5dB step size/ Gain index. So, each increment or decrement of Gain index will be 0.5dB step from its current value

    3A) Its possible to set the initial gain index using SPI mode and then switch to PIN control mode

    4A) You can readback the Gain index by using adi_adrv9025_RxGainGet() irrespective of the gain control mode.

  • Thank you Ramarao for the answers.

    If i use default gain table, how is the gain range i can control with GPIOs?

    I tested rxGainIndex from 190 to 255 and can see over 50dB gain range, can i have the same range with GPIO pin control?

    Thanks.

Reply Children