Post Go back to editing

Duration calculation in Power Amplifier Protection

Category: Software
Product Number: ADRV9029
Software Version: 6.4.0.14

There are avgDuration and peakDuration setting in PA protection function.

As for avgDuration, what does "L" mean?

If the txSampleRate=122.88MHz, avgDuration is set to 10, then what is the time of duration in seconds?

From the formula, there is "5" added, does it mean the least duration is 5 seconds?

Could you teach me how to calculate the real duration time? 

Thanks.