mother board : ADS9-V2EBZ
Daughter board:ADRV9029-HB/PCBZ
ADRVTRX Transceiver Evaluation Software Version: 6.4.0.17
HI ADI Engineer!
i choose to input a waveform file instead of using the internal NCO by selecting the LoadFile checkbox and entering the path to the waveform file.

However, After Pressing the play symbol,the following error occurred:
2024-10-10 02:31:04,388 [ERROR] ERROR PerformTx() failed. Exception message: Index was outside the bounds of the array.
---------- EXCEPTION: ----------
System.IndexOutOfRangeException: Index was outside the bounds of the array.
at System.Array.InternalGetReference(Void* elemRef, Int32 rank, Int32* pIndices)
at System.Array.GetValue(Int32 index)
at adrv9010_dll.SubClasses.Fpga9010TxExt.TransportSet(adi_fpga9010_JesdInfo_t jesdInfo, Byte[] dataBytes, List`1& data)
at adrv9010_dll.SubClasses.Fpga9010TxExt.TxDataSet(adi_fpga9010_JesdInfo_t jesdInfo, adi_fpga9010_TxDatamoverSel_e txDatamoverSel, List`1 data)
at adrv9010_dll.TopLevelClasses.AdrvDaughterCard.PerformTx(adi_fpga9010_TxTollgateTrigSources_e trigSource, List`1 txData, UInt32 channelMask, Byte continuous)
at Adi.Trx.Adrv9xxx.Adrv9xxxApiCommon.PerformTx(List`1 dataArray, CaptureTrigger trigger)
------------------------------
System.IndexOutOfRangeException: Index was outside the bounds of the array.
at System.Array.InternalGetReference(Void* elemRef, Int32 rank, Int32* pIndices)
at System.Array.GetValue(Int32 index)
at adrv9010_dll.SubClasses.Fpga9010TxExt.TransportSet(adi_fpga9010_JesdInfo_t jesdInfo, Byte[] dataBytes, List`1& data)
at adrv9010_dll.SubClasses.Fpga9010TxExt.TxDataSet(adi_fpga9010_JesdInfo_t jesdInfo, adi_fpga9010_TxDatamoverSel_e txDatamoverSel, List`1 data)
at adrv9010_dll.TopLevelClasses.AdrvDaughterCard.PerformTx(adi_fpga9010_TxTollgateTrigSources_e trigSource, List`1 txData, UInt32 channelMask, Byte continuous)
at Adi.Trx.Adrv9xxx.Adrv9xxxApiCommon.PerformTx(List`1 dataArray, CaptureTrigger trigger)
Please Clear Logs and API errors and try again.
This is the waveform file I used.Whether the file format is required?
Tx_LTE_245.76Msps_1Carrier.txt
Thanks!