Post Go back to editing

Bandwidth Configuration Question

Category: Software
Product Number: ADRV9029
Software Version: 6.4.0.14

We have a new project and the requirement is:

   Signal Bandwidth: 12MHz

   Sample Rate: 20.48Msps

We are checking the profile to match it and see 44_nonlinkSharing is the most close scheme.

However, the Tx sample rate(61.44M), Tx bandwidth(40M) and Rx sample(61.44M) rate are much higher than our requirement.

1) So for next step, what should we do to meet the requirement?

2) Shall we modify the profile(rx/tx sample rate, bandwith) based on 44_nonlinkSharing?

3) What is the minimum value for rx/tx RF bandwidth and sample rate? We just see maximum value in UG but no minimum value specified.

Parents Reply Children
No Data