Post Go back to editing

CpuBootStatus_e: 6 - Bootup clkgen setup error.

Category: Software
Product Number: adrv9026
Software Version: ADRV9025 API Version: 6.4.0.14

We used to use a 51_nonlinksharing profile and 9528 provided a 245.76M clock to 9026. Now that we have changed the profile to 61_linksharing, the following clock error appears. Do we need to modify the clock provided by 9528 to 9026 after changing the profile?

Error log:

2023-01-01 08:58:07: API_LOG:adi_adrv9025_CpuMemWrite(...)
2023-01-01 08:58:07: API_LOG:adi_adrv9025_CpuStart(...)
2023-01-01 08:58:07: API_LOG:adi_adrv9025_CpuMemWrite(...)
2023-01-01 08:58:07: API_LOG:adi_adrv9025_ConfigFileLoad(...)
2023-01-01 08:58:07: API_LOG:adi_adrv9025_PreMcsInit_NonBroadCast(...)
2023-01-01 08:58:07: API_LOG:adi_adrv9025_CpuStartStatusCheck(...)
2023-01-01 08:58:07: ERROR:Error number 302120966 (0x12020006), Recovery action -2.In file public/src/adi_adrv9025_cpu.c, in function adi_adrv9025_CpuStartStatusCheck, in line 314, variable name device.Error message CpuBootStatus_e: 6 - Bootup clkgen setup error.

2023-01-01 08:58:07: ERROR:Error number 3 (0x00000003), Recovery action -2.In file public/src/adi_adrv9025_utilities.c, in function adi_adrv9025_PreMcsInit_NonBroadCast, in line 1687, variable name ((void *)0).Error message CpuBootStatus_e: 6 - Bootup clkgen setup error.

Thread Notes