Hello ADI Team,
Below is a portion of the 'ADRV9026/ADRV9029 Release Build Software Release Notes SW6.4.0.19'.
In the table above, the highlighted parts correspond to the DPD specific profile.
The Tx data rate is set to 122.88MSPS or higher.
Is it not possible to use DPD with a data rate lower than this?
If it is not possible to use DPD with a Tx data rate lower than 122.88MSPS, could you explain the reason to me?
For your reference, I would like to use 61.44MSPS for a bandwidth of 50MHz.
I look forward to your response.
Best regards,
Paul
add comment
[edited by: PaulJung at 8:52 AM (GMT -4) on 9 Jul 2024]