Post Go back to editing

adrv9026 CPU exception for any API call after initialization

Category: Software
Product Number: ADRV9026

Versions used:

Adi.Adrv9025.GainTables 6.4.0.1
Adi.Adrv9025.Api 6.4.0.14
Adi.Adrv9025.Firmware 6.4.0.6
Adi.Adrv9025.Gui 6.4.0.17

============

After Madura initialization, my jesd link is up, and I can receive correct data over the link. However, any subsequent command that involves the CPU results in an exception. 

adi_adrv9025_CpuCmdWrite.1308: cpuCommandBusy = 0
adi_adrv9025_CpuCmdStatusWait.1115: CPU event checks exceeded max 1000
adi_adrv9025_CpuCmdStatusWait.1137: CPU exception ffffffff

A second attempt would fill console reporting CPU busy = 1

The APIs that I have tried: adi_adrv9025_pllFrequencyGet, adi_adrv9025_pllFrequencySet, adi_adrv9025_RxNcoShifterSet/Get, adrv9025_calsInit etc. My primary goal is to enable and shift the bank A NCO1 to tune to the carrier.

Is there any procedure prior to issuing the APIs? I tried disabling RX/TX with no luck. Rerunning PostMCSInit also fails as it involves CPU commands.

Any help or suggestion would be greatly appreciated.

Thanks

Sharif

Parents Reply Children
  • It's an issue with all APIs.
    UPDATE: I placed the NCO shift function at various stages in initialization, and found that it works prior to  calling adi_adrv9025_TrackingCalsEnableSet function. The tracking Cals command is probably messing up something in the CPU, although it returns no error. I commented out that code for the time being and I can now call any API, such as LO frequency set, etc. during runtime.