Post Go back to editing

Tx/Rx Signal bandwidth

Category: Software
Product Number: adrv9029
Software Version: 6.4.0.14

Hi Dear,

We are using ADRV9029, the requirement is sampling rate 122.88MHz, but the actual baseband signal is 30MHz bandwidth.

I see that in the GUI, there is no 30MHz bandwith profile list.

How can i set the bandwith to 30MHz? I have concern that if i use primary signal BW 100MHz from profile the filters would not be narrow enough for my actual signal BW.

Thanks!

Parents Reply Children
No Data