(1) When we use ADRV9026 use case 44 configuration, we are unable to update graphs,We will directly apply the Use case 44 configuration to the project, but the power consumption is too high. How can we reduce power consumption under this configuration?
How to change the filter order in the configuration?
(2)We adjusted the parameters of use case 44, and the software can update Graphs and Gernate Profile. However, our board was powered on multiple times and found that the Tx phase was unstable, with a jump of about 10 degrees. How can we solve this problem?
The parameters we adjusted are:
Tx Input Sample Rate 61.44
Tx RF Synthesis Bandwidth 48
Tx Primary Signal BW 40
ORx RF Bandwidth 45
choose DPD HB1 Enable
choose DPD HB2 Enable
Tx int factor 8
Rx Dec factor 32
ORx Dec factor 20
thanks!