Post Go back to editing

ADRV9026 multi-chip phase synchronization

Category: Software

We had a question when implementing phase synchronization with the ADRV9026:

Do the phase differences of multiple channels of an ADRV9026 change after the LO local frequency is changed? For example, when the local oscillator is set to 1Ghz, the phase difference between RX1 and RX2 is 10°, then when the local oscillator is modified to 2GHz or other frequencies, the phase difference between RX1 and RX2 should still be 10°?