Post Go back to editing

How can i get the ADRV9026 or ADRV9029 FPGA project?

Category: Software
Product Number: ADRV9026 ADRV9029

Hi, my friends,

    I got an EVAL-ADRV9026/ADRV9029 and connected it with ZC706. So far, ZC706 could control the ad9528 and adrv9029 of the board with Spi interface.

    But now, i wonna debug the adrv9029, for example, i hope to change the Sample rate from 122.88Mhz to 30.72Mhz(of course , some other paramaters should be changed relatively). But i can not get the FPGA project.

    So, my questions are:

    1. Where can i get the FPGA Project (Like adrv9009).

    2. If the adrv9029 FPGA project is not open source, where can i get the .bit or .bin file of the Fpga Project, which could be used directly like a black box?