Post Go back to editing

ADRV9026 JESD ORx Data Source Select

Thread Summary

The user is confused about selecting ORx data sources for the JESD Framer, noting only two data paths for four ORx channels. The final answer clarifies that ORX1 and ORX2 RF channels are multiplexed onto a single ORX BB channel, and the same applies to ORX3 and ORX4. The default source for ORX1 BB is ORX1, and for ORX2 BB is ORX3. To change the source, use the ORX API mode to select the desired RF channel.
AI Generated Content
Category: Software
Product Number: ADRV9026
Software Version: 6.4.0.14

Hi,

I 'm confused about the ORx data source to send into the JESD Framer.

 

As shown above, there are only two data paths for ORx data and there are four ORx channel. 

How can I choose the data source for each ORx data path to send into the JESD Framer? For example, I want to check the ORx3 and ORx4 data and I want to set ORx3 as the data source for ORx1_IQ, ORx4 for ORx2_IQ. What should I do?

Thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.