Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ADRV9040 - Multi-band capability

Category: Hardware
Product Number: ADRV9040

Hi,

I am working with a customer that is working with the following 7 bands. Note that they are acting as a UE, not a base station, because they are doing monitoring applications: 

  • Band 28 (RX: 758 - 788 MHz, TX: 703-733 MHz)
  • Band 20 (RX: 791-821MHz, TX: 832 - 862 MHz)
  • Band 8: (RX: 925 - 960 MHZ, TX: 880 - 915 MHz)
  • Band 3: (RX: 1805-1880 MHz, TX: 1710-1785 MHz)
  • Band 1: (RX: 2110 - 2170 MHz, TX: 1920 - 1980 MHz)
  • Band 7: (RX: 2620 - 2690 MHz, TX: 2500 - 2570MHz)
  • Band 78: (TDD 3400 - 3800 MHz)

From the data sheet I see the following note: It allows up to 4 bands within the range : 650 MHz to 6 GHz

It means they need 2x ADRV9040 to do this, right?

Thanks

Alex

Edit Notes


[locked by: Ramarao at 3:20 PM (GMT -4) on 12 Jul 2023]