Post Go back to editing

Question on how to receive ORX data through JESD after DPD operation in ADRV9029

Category: Software
Product Number: ADRV9029
Software Version: SW6.2.0.35

It is set to 3pin ORx Selection mode as shown in the figure below.

However, although I enabled it on the RXx_en pin, ORx Data is not coming in through JESD.

I know that no ORX data is coming out through JESD during DPD operation.

But I want to receive ORX data through JESD when DPD operation is finished, please advise on how to control it.

Thank you for your support.

Edit Notes

add
[edited by: Justin.Jung at 2:23 AM (GMT -4) on 27 Jun 2022]
Parents
  • However, although I enabled it on the RXx_en pin, ORx Data is not coming in through JESD.

    You are using a link sharing profile so the ORX data comes on JESD only when the TX is on.

    I know that no ORX data is coming out through JESD during DPD operation.

    Yes, but the other ORX side of the chip can get the JESD data.

    See below:

    When ORX_CTRL_A is high and based on CTRL_B and CTRL_C logics, the respective ORX data goes to the JESD and on the other ORX side of the chip, the DPD cal will run.

Reply
  • However, although I enabled it on the RXx_en pin, ORx Data is not coming in through JESD.

    You are using a link sharing profile so the ORX data comes on JESD only when the TX is on.

    I know that no ORX data is coming out through JESD during DPD operation.

    Yes, but the other ORX side of the chip can get the JESD data.

    See below:

    When ORX_CTRL_A is high and based on CTRL_B and CTRL_C logics, the respective ORX data goes to the JESD and on the other ORX side of the chip, the DPD cal will run.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.