Hi AD support,
I'm trying to have some preliminary DPD tests with ADS9-V2EBZ + EVAL-ADRV9029-HB on TES-GUI-6.3.0.5. I'm using profile 50 Link sharing, Tx input rate 122.88MHz, and thus 1228800 samples for 10ms signal input. However, while connecting my spectrum analyzer right to the Tx output, it shows a very noisy constellation:

This is my original LTE signal:

And this is the signal shown in TES GUI, seems to be clean and no clipping:

After some initial debug efforts, the IQ offset shown in VSA is very high, which could be related to carrier feedthrough. Therefore, I suspect that I'm missing some configurations or RF chain calibrations.
My signal can be found attached: modulated_readback_Tx1.txt
My VSA setup can be found attached: LTE_DL_20MHz_DEMOD_ConstellationView3.zip
Edit Notes
fix typos, add VSA setx[edited by: MasonH at 2:00 AM (GMT -4) on 29 Apr 2022]