Hi All
I have ADRV9029/26 EVB depend on guide the power can be +_6dbm max how can i change the power output from TX port in 9026?Please
Best Regards
Hi All
I have ADRV9029/26 EVB depend on guide the power can be +_6dbm max how can i change the power output from TX port in 9026?Please
Best Regards
Whats your DPD tracking calibration configuration? You can try optimising the parameters such as Regularization value, Peak search window size, change the DPD update mode (2 for GaN PA) etc. Also, you may do a model sweep to identify the best model for your PA
Hi Ramarao
I was going through ADRV9029 data sheet and have found following paragraph page(128):
"The DPD is optimized for power amplifiers with rms output powers in the 250 mW to 10 W range"
I need to used for two amplifiers in a balanced configuration for get 42dBm (ideally), it will be higher than 10w. will DPD be still working for this power level?
Yes, there is no such restriction on the output power level from the DPD perspective. DPD will work for your target output power.
many thanks
Hi Ramarao
1-DPD tracking calibration configuration? how many mode for calibration we have
2- how to set the "Regularization value"? Please
3- How to set the "Peak search window size"?
Best Regards
Rich
Hi aarontah
How to change IF GAIn to Low?Please
Best Regards
Rich
Regularization value, Peak search window size,
Hi all
I have this configuration as shown below
I set my signal Generator 3.5Ghz and 100Bandwith
which is received by ADRV _RX1
and I transmitted by using TX1 as shown before
The problem when I tried revive the signal through the ORX1 by suing TES software
when i switch ORX on i got
and
I lost signal from TX1 direct
please could you help me why this happen and how to avoid this error?
Best Regards
Rich
Is your TX output is connected back to ORX path?
Can you just feed an RF signal at the ORX input and check if the spectrum is observed in the GUI?
The TX should not disappear when ORX is ON, can you check if the RX got turned off by mistake from the sig. gen?
Hi Ramarao
Is your TX output is connected back to ORX path? Yes mate
Can you just feed an RF signal at the ORX input and check if the spectrum is observed in the GUI? I working on these
The TX should not disappear when ORX is ON, can you check if the RX got turned off by mistake from the sig. gen?(TX on because i can see the o/p in spectrum analyzer.)
TX-ON, RX-ON just when i switch on ORX every thing change to off.
an you just feed an RF signal at the ORX input and check if the spectrum is observed in the GUI?
TDD Case
FDD Signal