Hi All
I have ADRV9029/26 EVB depend on guide the power can be +_6dbm max how can i change the power output from TX port in 9026?Please
Best Regards
Hi All
I have ADRV9029/26 EVB depend on guide the power can be +_6dbm max how can i change the power output from TX port in 9026?Please
Best Regards
The full scale output power of the TRX is as below:
You can use Tx. attenuation control to change the Tx power.
BTW,Where from are you referring to +/-6dBm?
Hi all
I have this configuration as shown below
I set my signal Generator 3.5Ghz and 100Bandwith
which is received by ADRV _RX1
and I transmitted by using TX1 as shown before
The problem when I tried revive the signal through the ORX1 by suing TES software
when i switch ORX on i got
and
I lost signal from TX1 direct
please could you help me why this happen and how to avoid this error?
Best Regards
Rich
Is your TX output is connected back to ORX path?
Can you just feed an RF signal at the ORX input and check if the spectrum is observed in the GUI?
The TX should not disappear when ORX is ON, can you check if the RX got turned off by mistake from the sig. gen?
Hi Ramarao
Is your TX output is connected back to ORX path? Yes mate
Can you just feed an RF signal at the ORX input and check if the spectrum is observed in the GUI? I working on these
The TX should not disappear when ORX is ON, can you check if the RX got turned off by mistake from the sig. gen?(TX on because i can see the o/p in spectrum analyzer.)
TX-ON, RX-ON just when i switch on ORX every thing change to off.
Hi Ramarao
Is your TX output is connected back to ORX path? Yes mate
Can you just feed an RF signal at the ORX input and check if the spectrum is observed in the GUI? I working on these
The TX should not disappear when ORX is ON, can you check if the RX got turned off by mistake from the sig. gen?(TX on because i can see the o/p in spectrum analyzer.)
TX-ON, RX-ON just when i switch on ORX every thing change to off.