Hi All
I have ADRV9029/26 EVB depend on guide the power can be +_6dbm max how can i change the power output from TX port in 9026?Please
Best Regards
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
Hi All
I have ADRV9029/26 EVB depend on guide the power can be +_6dbm max how can i change the power output from TX port in 9026?Please
Best Regards
The full scale output power of the TRX is as below:

You can use Tx. attenuation control to change the Tx power.
BTW,Where from are you referring to +/-6dBm?
Dear Ramarao
Many thanks for your answer, but max what i can obtained of board -10 dbm whem i used the waveform or 2 tones abd ATT =0 for TX1.
Best Regards
Richs1
What is the raw ACLR of the PA? How much correction are you getting?
Can you please provide us the DPD tracking config. parameters and the DPD statistics?
What is the ORX gain Index?
Can you please test at 3dB backoff from the target power and check the DPD performance?
Hi Rammaro
Many thank for your help,DPD is working now.
Please could you guide me how can i receive signal from Signal generator--->ADRV board(RX)------>ADRV board TX port by using GUI.
Best Regards
Please use the attached script for the Rx to Tx loop back. If you are measuring EVM, make sure to swap the IQ in Spectrum Analyser.
Many thanks,
the steps will be
1- run the .py scripts
2-Run DPD after that.
Best Regards
Yes. Could you please let me know what are you trying to test/ achieve with the loop back test? Are you trying to measure the RX performance? If so, i would advice to test at the Tx out of the chip rather testing at PA out.
Hi
I tried to make DPD work with 5G signal BW100 MHz
the problem I tried to generate signal by using MATLAB but look like the signal has distortion therefore i change my cct. to
I try to approve the concept of DPD work with 5G
Best Regards
Hi Rammarao
Many thanks for your help,I can pass the signal rx tp tx
Hi Ramarao
when i send the signal direct from signal generator to PA
but when I send through ADRV I got

when i send the signal direct from signal generator to PA
You mean directly from the signal generator to the PA input, no ADRV involved? Which Test model is this?
but when I send through ADRV I got
Can you check at lower powers, may be about 3dB backoff and see if the spectrum is fine?
Are you measuring with the same test model as above?
I believe the input signal to Rx. input is within the dynamic range and not saturating the Rx path?
Try to provide RF input somewhere around -25dBm or so at the Rx. input.
when i send the signal direct from signal generator to PA
You mean directly from the signal generator to the PA input, no ADRV involved? Which Test model is this?
but when I send through ADRV I got
Can you check at lower powers, may be about 3dB backoff and see if the spectrum is fine?
Are you measuring with the same test model as above?
I believe the input signal to Rx. input is within the dynamic range and not saturating the Rx path?
Try to provide RF input somewhere around -25dBm or so at the Rx. input.


before DPD

after DPD

any possibility to increase the correction to obtain -47 or-50 dbc
please?
You may try to change "IF GAIN" from “LOW” to “medium”
Whats your DPD tracking calibration configuration? You can try optimising the parameters such as Regularization value, Peak search window size, change the DPD update mode (2 for GaN PA) etc. Also, you may do a model sweep to identify the best model for your PA
Hi Ramarao
I was going through ADRV9029 data sheet and have found following paragraph page(128):
"The DPD is optimized for power amplifiers with rms output powers in the 250 mW to 10 W range"

I need to used for two amplifiers in a balanced configuration for get 42dBm (ideally), it will be higher than 10w. will DPD be still working for this power level?
Yes, there is no such restriction on the output power level from the DPD perspective. DPD will work for your target output power.
many thanks
Hi Ramarao
1-DPD tracking calibration configuration? how many mode for calibration we have
2- how to set the "Regularization value"? Please
3- How to set the "Peak search window size"?
Best Regards
Rich
Hi aarontah
How to change IF GAIn to Low?Please
Best Regards
Rich
Regularization value, Peak search window size,