Post Go back to editing

ADRV9029/26 EVB Power

Hi All

I have ADRV9029/26 EVB depend on guide the power can be +_6dbm max how can i change the power output from TX port in 9026?Please

Best Regards

Parents Reply
  • At what frequency, are you measuring the output power? The EVB that you have is matched for Low band, Mid band or high band?

    The output power also depends on the BB input waveform scaling that you are using.

    For eg, if the PAR of the input waveform signal is 11dB and if you use -11dBFS scaling waveform, you could get an output power of 7(Max. power)-11 = -4dBm from the Tx.out.

    Try testing with a CW tone initially.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.