ADRV9029
Recommended for New Designs
The ADRV9029 is a highly integrated, radio frequency (RF) agile transceiver offering four independently controlled transmitters, dedicated observation...
Datasheet
ADRV9029 on Analog.com
Hello,
I have a ton of questions to ask about DPD configuration on the ADRV9025 chip. I am trying to configure DPD without the PA connected between the Tx-ORx path solely for testing purposes. I have gone through all the steps required in setting up DPD but there seems to be no signal in the ORx path. The dpdErrorCode I get shifts between 0x3405 and 0x340E.
My setup is as follows:
I am running a 2T-2R-2ORx setup utilizing TX3/TX2, RX3/RX2, and ORX3/ORX1. With this setup, I am running DPD on the TX2, connecting the output of the TX2 via a splitter to the ORX1 port and a spectrum analyzer (So as to monitor the TX2-ORX1 path).
For the DPD Tracking Cal Bring up Sequence, I followed the following steps. Note that I have supplied only the necessary snippets to avoid cluttering up this page:
1a. Program the device and run initial calibrations
1b. Run TxQEC initial calibration after chip initialization (for some reason, the programming failed when I tried to run the tx_qec init cal as part of the POSTMCS during initialization, see code snippet)
recoveryAct = adi_init_tx_cals_run( adrv9025Device,
ADI_ADRV9025_TX2,
( ADI_ADRV9025_TX_QEC_INIT | ADI_ADRV9025_INTERNAL_PATH_DELAY | ADI_ADRV9025_TX_LO_LEAKAGE_INTERNAL )
) ;
2. Disabled ORX channels mapped TX2 to ORX1 and called the adi_adrv9025_RadioCtrlCfgSet function, setting all control modes to SPI (see code snippet)
printf("*** Disabling ORx Channels ***\n") ;
recoveryAct = adi_adrv9025_RxTxEnableSet ( adrv9025Device, 0x06, 0x06 ) ;
rxChannelMaskGet = 0 ;
txChannelMaskGet = 0 ;
usleep(1) ;
recoveryAct = adi_adrv9025_RxTxEnableGet(adrv9025Device, &rxChannelMaskGet, &txChannelMaskGet) ;
recoveryAct = adi_adrv9025_TxToOrxMappingSet(device,ADI_ADRV9025_ORX1, ADI_ADRV9025_TX2);
adrv9025PostMcsInitInst.radioCtrlInit.radioCtrlModeCfg.orxRadioCtrlModeCfg.orxEnableMode = ADI_ADRV9025_ORX_EN_SPI_MODE; //ADI_ADRV9025_ORX_EN_SINGLE_CH_2PIN_MODE;
adrv9025PostMcsInitInst.radioCtrlInit.radioCtrlModeCfg.rxRadioCtrlModeCfg.rxEnableMode = ADI_ADRV9025_RX_EN_SPI_MODE ; //ADI_ADRV9025_RX_EN_PIN_MODE;
adrv9025PostMcsInitInst.radioCtrlInit.radioCtrlModeCfg.txRadioCtrlModeCfg.txEnableMode = ADI_ADRV9025_TX_EN_SPI_MODE ;//ADI_ADRV9025_TX_EN_PIN_MODE;
recoveryAct = adi_adrv9025_RadioCtrlCfgSet(adrv9025Device, &adrv9025PostMcsInitInst.radioCtrlInit.radioCtrlModeCfg);
3. Adjusted ORX1 gain, using gain index of 0xFF (see code snippet)
rx_gain.gainIndex = 0xFF ;
rx_gain.rxChannelMask = ADI_ADRV9025_ORX1 ;
recoveryAct = adi_adrv9025_RxGainSet (device, &rx_gain, 1);
4. Run the external path delay for TX2 (see code snippet)
adrv9025PostMcsInitInst.initCals.calMask = 0x00200000; //external path delay
adrv9025PostMcsInitInst.initCals.channelMask = ADI_ADRV9025_TX2 ;
adrv9025PostMcsInitInst.initCals.warmBoot = 0 ;
recoveryAct = adi_adrv9025_InitCalsRun(device, &adrv9025PostMcsInitInst.initCals);
recoveryAct = adi_adrv9025_InitCalsWait(device, 60000, &initCalsError);
5. Run the Tx external LOL init cals (see code snippet)
adrv9025PostMcsInitInst.initCals.calMask = 0x00000800; //external LOL adrv9025PostMcsInitInst.initCals.channelMask = ADI_ADRV9025_TX2 ; adrv9025PostMcsInitInst.initCals.warmBoot = 0 ; recoveryAct = adi_adrv9025_InitCalsRun(device, &adrv9025PostMcsInitInst.initCals); recoveryAct = adi_adrv9025_InitCalsWait(device, 60000, &initCalsError);
6. Configured the CFR settings (adi_adrv9025_CfrCtrlConfigSet, adi_adrv9025_CfrCorrectionPulseWrite_v2, adi_adrv9025_CfrEnableSet, adi_adrv9025_CfrHardClipperConfigSet, see code snippet)
7. Run the CFR Init Cals (with 60s wait time passed to the adi_adrv9025_InitCalsWait function)
8. Loaded the PA model (see code snippet)
dpdModelConfigInst.txChannelMask = ADI_ADRV9025_TX2 ;
dpdModelConfigInst.dpdNumFeatures = 22;
char* dpd_model = "/media/sddata/defaultDpdModel.txt" ;
FILE *fp = fopen(dpd_model, "r");
for(int n = 0; n <dpdModelConfigInst.dpdNumFeatures ; n++)
{
fscanf(fp, "%d %d %d %d %f %f",
&dpdModelConfigInst.dpdFeatures[n].i,
&dpdModelConfigInst.dpdFeatures[n].j,
&dpdModelConfigInst.dpdFeatures[n].k,
&dpdModelConfigInst.dpdFeatures[n].lut,
&dpdModelConfigInst.dpdFeatures[n].coeffReal,
&dpdModelConfigInst.dpdFeatures[n].coeffImaginary);
printf("\n%d %d %d %d %f %f\n",
dpdModelConfigInst.dpdFeatures[n].i,
dpdModelConfigInst.dpdFeatures[n].j,
dpdModelConfigInst.dpdFeatures[n].k,
dpdModelConfigInst.dpdFeatures[n].lut,
dpdModelConfigInst.dpdFeatures[n].coeffReal,
dpdModelConfigInst.dpdFeatures[n].coeffImaginary);
}
adi_adrv9025_TxChannels_e tx_channels ;
fclose(fp);
recoveryAct = adi_adrv9025_DpdModelConfigSet(adrv9025Device, &dpdModelConfigInst);
--- My DPD MODEL ---
0 0 0 0 0 0
0 0 1 0 0 0
0 0 2 0 0 0
0 0 3 0 0 0
0 0 4 0 0 0
0 0 5 0 0 0
1 1 1 2 0 0
1 1 2 2 0 0
1 1 3 2 0 0
1 1 4 2 0 0
1 1 5 2 0 0
0 1 0 8 0 0
0 1 1 8 0 0
0 1 2 8 0 0
0 1 3 8 0 0
0 1 4 8 0 0
0 1 5 8 0 0
2 2 1 26 0 0
2 2 2 26 0 0
2 2 3 26 0 0
2 2 4 26 0 0
2 2 5 26 0 0
9. Asserted DPD Reset (ADI_ADRV9025_DPD_RESET_FULL, see code snippet)
recoveryAct = adi_adrv9025_DpdReset(adrv9025Device, ADI_ADRV9025_TX2, ADI_ADRV9025_DPD_RESET_FULL);
if (recoveryAct != ADI_COMMON_ACT_NO_ACTION)
{
printf("ERROR: : %s:%u has failed.\n", __func__, __LINE__);
return recoveryAct;
}
10. Run DPD Tracking configuration (see code snippet)
int32_t MThreshold_dBFS = -21; int16_t DpdLowPowerThreshold_dBFS = -36; int16_t DpdLowPowerThresholdORx_dBFS = -36; int32_t temp = pow(10,(MThreshold_dBFS/20.0))*FULL_SCALE_CODE; int32_t dpdMThreshold_val = pow(temp,2); int16_t minAvgSignalLevel_val = pow(10,(DpdLowPowerThreshold_dBFS/20.0))*FULL_SCALE_CODE; int16_t minAvgSignalLevelOrx_val = pow(10,(DpdLowPowerThresholdORx_dBFS/20.0))*FULL_SCALE_CODE; dpdTrackingConfigInst.txChannelMask = ADI_ADRV9025_TX2; dpdTrackingConfigInst.minAvgSignalLevel = minAvgSignalLevel_val; dpdTrackingConfigInst.minAvgSignalLevelOrx = minAvgSignalLevelOrx_val; dpdTrackingConfigInst.dpdMThreshold = temp ; dpdTrackingConfigInst.dpdPeakSearchWindowSize = 65536; dpdTrackingConfigInst.dpdIndirectRegularizationValue = 30; dpdTrackingConfigInst.dpdDirectRegularizationValue = 30; dpdTrackingConfigInst.dpdSamples = 16384; dpdTrackingConfigInst.dpdUpdateMode = ADI_ADRV9025_DPD_TRACKING_UPDATE_MODE_0; dpdTrackingConfigInst.dpdIndirectRegularizationLowPowerValue = 20; dpdTrackingConfigInst.dpdFilterSel = 0; dpdTrackingConfigInst.enableDirectLearning = 0; dpdTrackingConfigInst.dpdMu = 50; recoveryAct = adi_adrv9025_DpdTrackingConfigSet(adrv9025Device, &dpdTrackingConfigInst);
11. Setup closed-loop gain control configurations (for monitoring purposes. See code snippet)
adi_adrv9025_ClgcConfig_t clgc_config ; clgc_config.clgcEnableGainControl = 0 ; clgc_config.txChannelMask = ADI_ADRV9025_TX2 ; recoveryAct = adrv9025_ClgcConfigSet( adrv9025Device, &clgc_config, 1) ;
12. Enabled TX QEC and TX LOL tracking Calibrations (See code snippet)
recoveryAct = adi_adrv9025_TrackingCalsEnableSet ( adrv9025Device,
( ADI_ADRV9025_TRACK_TX2_QEC | ADI_ADRV9025_TRACK_TX2_LOL ),
ADI_ADRV9025_TRACKING_CAL_ENABLE
);
13. Enabled DPD Tracking Calibration (See code snippet)
adi_adrv9025_TrackingCalsEnableSet (device, ADI_ADRV9025_TRACK_TX2_DPD, ADI_ADRV9025_TRACKING_CAL_ENABLE);
14. Enabled CLGC Tracking Calibration (See code snippet)
recoveryAct = adi_adrv9025_TrackingCalsEnableSet ( adrv9025Device,
ADI_ADRV9025_TRACK_TX2_CLGC,
ADI_ADRV9025_TRACKING_CAL_ENABLE
);
15. Started monitoring DPD tracking calibration (See code snippet)
//Wait for some time before getting the status
sleep(20);
adi_adrv9025_DpdStatus_t dpdStatus;
int32_t recoveryAction = 0;
recoveryAction = adi_adrv9025_DpdStatusGet (device, txChannel, &dpdStatus);
printf ("dpdErrorCode :0x%x\n",dpdStatus.dpdErrorCode);
printf ("dpdPercentComplete :%d\n",dpdStatus.dpdPercentComplete);
printf ("dpdPerformanceMetric :%d\n",dpdStatus.dpdPerformanceMetric);
printf ("dpdIterCount :%d\n",dpdStatus.dpdIterCount);
printf ("dpdUpdateCount :%d\n",dpdStatus.dpdUpdateCount);
printf ("dpdSyncStatus :%d\n",dpdStatus.dpdSyncStatus);
float meanTu = dpdStatus.dpdStatistics.dpdMeanTuPower;
float peakTu = dpdStatus.dpdStatistics.dpdPeakTuPower;
float meanTx = dpdStatus.dpdStatistics.dpdMeanTxPower;
float peakTx = dpdStatus.dpdStatistics.dpdPeakTxPower;
float meanOrx = dpdStatus.dpdStatistics.dpdMeanOrxPower;
float peakOrx = dpdStatus.dpdStatistics.dpdPeakOrxPower;
printf ("dpdModelTable :%d\n",dpdStatus.dpdModelTable);
printf ("dpdMeanTuPower :%f\n",20*log10(sqrt(meanTu) / 32768));
printf ("dpdPeakTuPower :%f\n",(20*log10(sqrt(peakTu) / 32768)));
printf ("dpdMeanTxPower :%f\n",(20*log10(sqrt(meanTx) / 32768)));
printf ("dpdPeakTxPower :%f\n",20*log10(sqrt(peakTx) / 32768));
printf ("dpdMeanOrxPower :%f\n",20*log10(sqrt(meanOrx) / 32768));
printf ("dpdPeakOrxPower :%f\n",20*log10(sqrt(peakOrx) / 32768));
printf ("dpdDirectEvm :%f\n",dpdStatus.dpdStatistics.dpdDirectEvm);
printf ("dpdIndirectEvm :%f\n",dpdStatus.dpdStatistics.dpdIndirectEvm);
printf ("dpdSelectError :%f\n",dpdStatus.dpdStatistics.dpdSelectError);
printf ("dpdIndirectError :%f\n",dpdStatus.dpdStatistics.dpdIndirectError);
printf ("dpdErrorStatus0 (metrics:actions): X:X :%d:%d\n", dpdStatus.dpdErrorStatus0.dpdMetricsMask,
dpdStatus.dpdErrorStatus0.dpdActionMask);
printf ("dpdErrorStatus1 (metrics:actions) :%d:%d\n", dpdStatus.dpdErrorStatus1.dpdMetricsMask,
dpdStatus.dpdErrorStatus1.dpdActionMask);
printf ("dpdPersistentErrorStatus0 (metrics:actions) :%d:%d\n", dpdStatus.dpdPersistentErrorStatus0.dpdMetricsMask,
dpdStatus.dpdPersistentErrorStatus0.dpdActionMask);
printf ("dpdPersistentErrorStatus1 (metrics:actions) :%d:%d\n", dpdStatus.dpdPersistentErrorStatus1.dpdMetricsMask,
dpdStatus.dpdPersistentErrorStatus1.dpdActionMask);
printf ("reservedPM :%d\n",dpdStatus.reservedPM);
printf ("reservedTP :%d\n",dpdStatus.reservedTP);
printf ("reservedPR :%d\n",dpdStatus.reservedPR);
16. Started monitoring CLGC status (See code snippet)
recoveryAct = adi_adrv9025_ClgcStatusGet( adrv9025Device ,
ADI_ADRV9025_TX2,
&clgc_status
);
printf("******** CLGC Monitoring ****************\n") ;
printf ("clgc_status.clgcLoopGain : %f\n", clgc_status.clgcLoopGain) ;
printf ("clgc_status.clgcTxRmsPower : %f\n", clgc_status.clgcTxRmsPower) ;
printf ("clgc_status.clgcOrxRmsPower : %f\n", clgc_status.clgcOrxRmsPower) ;
printf ("clgc_status.activeTxAttenIndex : 0x%x\n", clgc_status.activeTxAttenIndex) ;
printf ("clgc_status.activeOrxGainIndex : 0x%x\n", clgc_status.activeOrxGainIndex) ;
---- And, here's the output of the above code: -----
dpdErrorCode of 3405 refers to 'ORX signal being Too small' which means the ORX signal is not present/ out of threshold.
You have mentioned ORX disabled in Step2, is it enabled while you are running DPD tracking cal?
Also, while you are running ext. path delay cal, hope the PA is switched on.
Have you generated the Initdata.c from the latest GUI with the required ORX selection and used in your code?
Hello Ramarao
ORx is disabled while running DPD tracking Cal. Actually, it stays disabled.
As I mentioned, I have not connected a PA between the Tx2-ORx1 path yet. That is if you mean the external PA.
I generated the initdata.c some time back and haven't changed it since, so I am not sure if the software has been update since then. And, from the initdata.c file, I can see we are using framer[1] for ORx1_I/Q. Please see the below snippet from the framer[1] setting.
{ // framer[1]
0, // enableJesd204C
0, // bankId
1, // deviceId
0, // lane0Id
2, // jesd204M
32, // jesd204K
4, // jesd204F
16, // jesd204Np
0, // jesd204E
1, // scramble
4, // serializerLanesEnabled
0, // lmfcOffset
1, // syncbInSelect
0, // overSample
1, // syncbInLvdsMode
0, // syncbInLvdsPnInvert
{ // serializerLaneCrossbar
8, // lane0FramerOutSel
8, // lane1FramerOutSel
0, // lane2FramerOutSel
8 // lane3FramerOutSel
},
{ // adcCrossbar
ADI_ADRV9025_ADC_ORX1_I, // conv0
ADI_ADRV9025_ADC_ORX1_Q, // conv1
ADI_ADRV9025_ADC_DISABLE, // conv2
ADI_ADRV9025_ADC_DISABLE, // conv3
ADI_ADRV9025_ADC_DISABLE, // conv4
ADI_ADRV9025_ADC_DISABLE, // conv5
ADI_ADRV9025_ADC_DISABLE, // conv6
ADI_ADRV9025_ADC_DISABLE, // conv7
ADI_ADRV9025_ADC_DISABLE, // conv8
ADI_ADRV9025_ADC_DISABLE, // conv9
ADI_ADRV9025_ADC_DISABLE, // conv10
ADI_ADRV9025_ADC_DISABLE, // conv11
ADI_ADRV9025_ADC_DISABLE, // conv12
ADI_ADRV9025_ADC_DISABLE, // conv13
ADI_ADRV9025_ADC_DISABLE, // conv14
ADI_ADRV9025_ADC_DISABLE, // conv15
ADI_ADRV9025_ADC_DISABLE, // conv16
ADI_ADRV9025_ADC_DISABLE, // conv17
ADI_ADRV9025_ADC_DISABLE, // conv18
ADI_ADRV9025_ADC_DISABLE, // conv19
ADI_ADRV9025_ADC_DISABLE, // conv20
ADI_ADRV9025_ADC_DISABLE, // conv21
ADI_ADRV9025_ADC_DISABLE, // conv22
ADI_ADRV9025_ADC_DISABLE // conv23
},
I may have to edit it so it supports ORx3 (since we are using that too. But, that should not be a problem since I am using the ORx1 right?
ORx is disabled while running DPD tracking Cal. Actually, it stays disabled.
ORX path must be enabled while DPD tracking cal is running.
As I mentioned, I have not connected a PA between the Tx2-ORx1 path yet. That is if you mean the external PA.
Oh yes, I missed that the PA is not connected in your setup.But the ORX path must be enabled for External Path delay cal.
Can you please generate the required configuration from the TES GUI and then use it?
ORx is disabled while running DPD tracking Cal. Actually, it stays disabled.
ORX path must be enabled while DPD tracking cal is running.
As I mentioned, I have not connected a PA between the Tx2-ORx1 path yet. That is if you mean the external PA.
Oh yes, I missed that the PA is not connected in your setup.But the ORX path must be enabled for External Path delay cal.
Can you please generate the required configuration from the TES GUI and then use it?
Hello Ramarao
Thank you for your response. I am a bit confused when you say I have to enable the ORX path while DPD cal is running because I got the idea of switching it off from another Analog devices employee. Kindly check Pvalavan's post from this link: https://ez.analog.com/wide-band-rf-transceivers/design-support-adrv9026/f/q-a/544898/adrv9029-dpd-configuration. I have quoted the part where I understood as I had to turn off the ORX pasth below:
"While testing DPD we recommend to disable the ORX Path. Before enabling DPD you can enable ORX path and measure ORXDecpower if required"
Could you kindly clarify for me? In the mean time, I will go ahead and enable the ORX path and let you know what I get from it.
Also, I already generated the required configuration from the TES GUI. That's what I am using. The only thing missing is the ORX3 path which I didn't enable. I hope I can test without that path enabled for now.
Correction: As you are using API/ SPI mode for ORX control, the ARM takes care of enabling/ disabling the ORX while DPD cal is running. So, ORX path need not be enabled explicitly.
Also, I already generated the required configuration from the TES GUI. That's what I am using. The only thing missing is the ORX3 path which I didn't enable. I hope I can test without that path enabled for now.
Yes, this should not be a problem.
This issue is something to do with ORX mapping, are you testing in FDD or TDD mode, Which use case are you using?
Hello Ramarao
Thanks a lot for the clarification.
To answer your question, I am using Use Case 50 nonLink Sharing.
This issue is something to do with ORX mapping
I am beginning to think so too. The signal doesn't go off completely as in when the Tx channel is disabled. I see a low-powered single tone when my written data gets taken down. Could it be the system reverts to a different mapping during DPD reset and as it cannot detect any data, it just sends an internally generated carrier signal?
When I call adi_adrv9025_TxToOrxMappingGet() however, it returns with 0x2 which is TX2 and that is correct. Could it be a problem in my GUI configuration?
Kindly let me know If you would need other information about my TES GUI configuration. I can send you my files and pictures of the GUI configurations.
Can you please disable CLGC tracking cal and test only with DPD tracking cal enable?
Kindly let me know If you would need other information about my TES GUI configuration. I can send you my files and pictures of the GUI configurations.
Yes, please share your files, pictures of the GUI configurations.
Hello Ramarao
Please check the link below for my GUI configuration images and generated files.
https://drive.google.com/file/d/1fa2g6JW450Zu_EiTTun6RbaSbRuG-U6e/view?usp=sharing
About testing with only DPD cal enable, that was what I did the first time I tried running DPD. I thought I probably had to include CLGC in order for the capture timeout and ORx low power error messages to go away. The results then, and now are the same.
Thanks for sharing the files. Can you please change the following and try once?
As you are using the same frequency for LO1 (RX) and LO2 (TX), can you switch off LO1 and use same LO2 for RX as well? So LO1 will be off and LO2 is used for both RX and TX.
Also, the ORX channel for TX2 need to be selected as ORX1 as per your Tx-ORX mapping.

Hello Ramarao
I tried what you suggested, the situation remains the same as before :(
I have a few questions though, I need to be sure about some things:
Have you connected the Tx2 path to ORX1 path without any switch between ORX1 and ORX2? Can you please send us the block diagram of the Physical connections including the control pins if you are using any for external ORX switch control, Selection etc.
What switch are you referring to? The configuration I used was the SPI mode for all channels. I enabled and disabled ORx/Tx/Rx via API. And you mentioned that the ARM CPU would do the switching (which is why I need not enable the ORx while running DPD tracking cals). This was before I switched to pin control mode (but that is still under test... I am using 2Tx/2Rx/2ORx and ORx mode is set to single-channel-2pin mode... still no luck, but I am testing)
I believe you are using custom board. If so, at what stage are you enabling the carrier. Can you try 'Reset DPD' and then enable the carrier? Can you read ORX dec power ?
Can you test it on EVB once? The ORX port naming is incorrect on the EVB(Treat ORX1 as ORX2 and vice versa). While you enable DPD tracking, make sure that the ORX capture is not being played in the GUI.
Please refer to various use cases as mentioned in Page 114 of the user guide.