KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
ADRV9026
Recommended for New Designs
The ADRV9026 is a highly integrated, radio frequency (RF) agile transceiver offering four independently controlled transmitters, dedicated observation...
Datasheet
ADRV9026 on Analog.com
The user can refer to the “RECEIVER GAIN CONTROL AND GAIN COMPENSATION” section in the user guide to get an insight into the Rx/ORx gain table architecture. The Rx and ORX gain table share the same architecture, however the user can load different gain table for the Rx path and the ORx path. The user can load different gain table for Rx or ORx using the API function adi_adrv9025_ RxGainTableWrite(). This function uses rxChannelMask as one of the input parameters with which the user can load a different gain table for the desired ORx channel. The default ORx gain table has 0.5dB step on ADI EVB system. The user can change the gain step from default 0.5dB to 1dB by removing every other FE Control Word & digital gain setting in the default gain table provided by ADI.
The front end attenuator has an 8-bit control word. The amount of attenuation applied depends on the value set in the front-end attenuator column of the selected gain table index. The following equation provides an approximate relationship between the internal attenuator and the front-end attenuation value programmed in the gain table, N:

The signed digital gain/attenuation is used to apply gain or attenuation digitally. The range of the digital gain is 0 to 50 dB. The range of the digital attenuation is 0 to 18 dB. The resolution of the steps is 0.05 dB. As an example, a value of 14 would result in 0.7 dB gain, and a value of -14 would result in 0.7 dB of attenuation.
If the user wants to set the ORx gain step to 1dB, they can use the sample ORx gain table as shown below. Please note that the gain table provided below has been optimized for accurate step size based on silicon characterization.
|
Gain Index |
FE Control Word |
TIA Control |
ADC Control |
Ext Control |
Phase Offset |
Digital Gain |
|
0 |
0 |
0 |
0 |
0 |
0 |
0 |
|
1 |
0 |
0 |
0 |
0 |
0 |
0 |
|
2 |
0 |
0 |
0 |
0 |
0 |
0 |
|
3 |
0 |
0 |
0 |
0 |
0 |
0 |
|
4 |
0 |
0 |
0 |
0 |
0 |
0 |
|
5 |
0 |
0 |
0 |
0 |
0 |
0 |
|
6 |
0 |
0 |
0 |
0 |
0 |
0 |
|
7 |
0 |
0 |
0 |
0 |
0 |
0 |
|
8 |
0 |
0 |
0 |
0 |
0 |
0 |
|
9 |
0 |
0 |
0 |
0 |
0 |
0 |
|
10 |
0 |
0 |
0 |
0 |
0 |
0 |
|
11 |
0 |
0 |
0 |
0 |
0 |
0 |
|
12 |
0 |
0 |
0 |
0 |
0 |
0 |
|
13 |
0 |
0 |
0 |
0 |
0 |
0 |
|
14 |
0 |
0 |
0 |
0 |
0 |
0 |
|
15 |
0 |
0 |
0 |
0 |
0 |
0 |
|
16 |
0 |
0 |
0 |
0 |
0 |
0 |
|
17 |
0 |
0 |
0 |
0 |
0 |
0 |
|
18 |
0 |
0 |
0 |
0 |
0 |
0 |
|
19 |
0 |
0 |
0 |
0 |
0 |
0 |
|
20 |
0 |
0 |
0 |
0 |
0 |
0 |
|
21 |
0 |
0 |
0 |
0 |
0 |
0 |
|
22 |
0 |
0 |
0 |
0 |
0 |
0 |
|
23 |
0 |
0 |
0 |
0 |
0 |
0 |
|
24 |
0 |
0 |
0 |
0 |
0 |
0 |
|
25 |
0 |
0 |
0 |
0 |
0 |
0 |
|
26 |
0 |
0 |
0 |
0 |
0 |
0 |
|
27 |
0 |
0 |
0 |
0 |
0 |
0 |
|
28 |
0 |
0 |
0 |
0 |
0 |
0 |
|
29 |
0 |
0 |
0 |
0 |
0 |
0 |
|
30 |
0 |
0 |
0 |
0 |
0 |
0 |
|
31 |
0 |
0 |
0 |
0 |
0 |
0 |
|
32 |
0 |
0 |
0 |
0 |
0 |
0 |
|
33 |
0 |
0 |
0 |
0 |
0 |
0 |
|
34 |
0 |
0 |
0 |
0 |
0 |
0 |
|
35 |
0 |
0 |
0 |
0 |
0 |
0 |
|
36 |
0 |
0 |
0 |
0 |
0 |
0 |
|
37 |
0 |
0 |
0 |
0 |
0 |
0 |
|
38 |
0 |
0 |
0 |
0 |
0 |
0 |
|
39 |
0 |
0 |
0 |
0 |
0 |
0 |
|
40 |
0 |
0 |
0 |
0 |
0 |
0 |
|
41 |
0 |
0 |
0 |
0 |
0 |
0 |
|
42 |
0 |
0 |
0 |
0 |
0 |
0 |
|
43 |
0 |
0 |
0 |
0 |
0 |
0 |
|
44 |
0 |
0 |
0 |
0 |
0 |
0 |
|
45 |
0 |
0 |
0 |
0 |
0 |
0 |
|
46 |
0 |
0 |
0 |
0 |
0 |
0 |
|
47 |
0 |
0 |
0 |
0 |
0 |
0 |
|
48 |
0 |
0 |
0 |
0 |
0 |
0 |
|
49 |
0 |
0 |
0 |
0 |
0 |
0 |
|
50 |
0 |
0 |
0 |
0 |
0 |
0 |
|
51 |
0 |
0 |
0 |
0 |
0 |
0 |
|
52 |
0 |
0 |
0 |
0 |
0 |
0 |
|
53 |
0 |
0 |
0 |
0 |
0 |
0 |
|
54 |
0 |
0 |
0 |
0 |
0 |
0 |
|
55 |
0 |
0 |
0 |
0 |
0 |
0 |
|
56 |
0 |
0 |
0 |
0 |
0 |
0 |
|
57 |
0 |
0 |
0 |
0 |
0 |
0 |
|
58 |
0 |
0 |
0 |
0 |
0 |
0 |
|
59 |
0 |
0 |
0 |
0 |
0 |
0 |
|
60 |
0 |
0 |
0 |
0 |
0 |
0 |
|
61 |
0 |
0 |
0 |
0 |
0 |
0 |
|
62 |
0 |
0 |
0 |
0 |
0 |
0 |
|
63 |
0 |
0 |
0 |
0 |
0 |
0 |
|
64 |
0 |
0 |
0 |
0 |
0 |
0 |
|
65 |
0 |
0 |
0 |
0 |
0 |
0 |
|
66 |
0 |
0 |
0 |
0 |
0 |
0 |
|
67 |
0 |
0 |
0 |
0 |
0 |
0 |
|
68 |
0 |
0 |
0 |
0 |
0 |
0 |
|
69 |
0 |
0 |
0 |
0 |
0 |
0 |
|
70 |
0 |
0 |
0 |
0 |
0 |
0 |
|
71 |
0 |
0 |
0 |
0 |
0 |
0 |
|
72 |
0 |
0 |
0 |
0 |
0 |
0 |
|
73 |
0 |
0 |
0 |
0 |
0 |
0 |
|
74 |
0 |
0 |
0 |
0 |
0 |
0 |
|
75 |
0 |
0 |
0 |
0 |
0 |
0 |
|
76 |
0 |
0 |
0 |
0 |
0 |
0 |
|
77 |
0 |
0 |
0 |
0 |
0 |
0 |
|
78 |
0 |
0 |
0 |
0 |
0 |
0 |
|
79 |
0 |
0 |
0 |
0 |
0 |
0 |
|
80 |
0 |
0 |
0 |
0 |
0 |
0 |
|
81 |
0 |
0 |
0 |
0 |
0 |
0 |
|
82 |
0 |
0 |
0 |
0 |
0 |
0 |
|
83 |
0 |
0 |
0 |
0 |
0 |
0 |
|
84 |
0 |
0 |
0 |
0 |
0 |
0 |
|
85 |
0 |
0 |
0 |
0 |
0 |
0 |
|
86 |
0 |
0 |
0 |
0 |
0 |
0 |
|
87 |
0 |
0 |
0 |
0 |
0 |
0 |
|
88 |
0 |
0 |
0 |
0 |
0 |
0 |
|
89 |
0 |
0 |
0 |
0 |
0 |
0 |
|
90 |
0 |
0 |
0 |
0 |
0 |
0 |
|
91 |
0 |
0 |
0 |
0 |
0 |
0 |
|
92 |
0 |
0 |
0 |
0 |
0 |
0 |
|
93 |
0 |
0 |
0 |
0 |
0 |
0 |
|
94 |
0 |
0 |
0 |
0 |
0 |
0 |
|
95 |
0 |
0 |
0 |
0 |
0 |
0 |
|
96 |
0 |
0 |
0 |
0 |
0 |
0 |
|
97 |
0 |
0 |
0 |
0 |
0 |
0 |
|
98 |
0 |
0 |
0 |
0 |
0 |
0 |
|
99 |
0 |
0 |
0 |
0 |
0 |
0 |
|
100 |
0 |
0 |
0 |
0 |
0 |
0 |
|
101 |
0 |
0 |
0 |
0 |
0 |
0 |
|
102 |
0 |
0 |
0 |
0 |
0 |
0 |
|
103 |
0 |
0 |
0 |
0 |
0 |
0 |
|
104 |
0 |
0 |
0 |
0 |
0 |
0 |
|
105 |
0 |
0 |
0 |
0 |
0 |
0 |
|
106 |
0 |
0 |
0 |
0 |
0 |
0 |
|
107 |
0 |
0 |
0 |
0 |
0 |
0 |
|
108 |
0 |
0 |
0 |
0 |
0 |
0 |
|
109 |
0 |
0 |
0 |
0 |
0 |
0 |
|
110 |
0 |
0 |
0 |
0 |
0 |
0 |
|
111 |
0 |
0 |
0 |
0 |
0 |
0 |
|
112 |
0 |
0 |
0 |
0 |
0 |
0 |
|
113 |
0 |
0 |
0 |
0 |
0 |
0 |
|
114 |
0 |
0 |
0 |
0 |
0 |
0 |
|
115 |
0 |
0 |
0 |
0 |
0 |
0 |
|
116 |
0 |
0 |
0 |
0 |
0 |
0 |
|
117 |
0 |
0 |
0 |
0 |
0 |
0 |
|
118 |
0 |
0 |
0 |
0 |
0 |
0 |
|
119 |
0 |
0 |
0 |
0 |
0 |
0 |
|
120 |
0 |
0 |
0 |
0 |
0 |
0 |
|
121 |
0 |
0 |
0 |
0 |
0 |
0 |
|
122 |
0 |
0 |
0 |
0 |
0 |
0 |
|
123 |
0 |
0 |
0 |
0 |
0 |
0 |
|
124 |
0 |
0 |
0 |
0 |
0 |
0 |
|
125 |
0 |
0 |
0 |
0 |
0 |
0 |
|
126 |
0 |
0 |
0 |
0 |
0 |
0 |
|
127 |
0 |
0 |
0 |
0 |
0 |
0 |
|
128 |
0 |
0 |
0 |
0 |
0 |
0 |
|
129 |
0 |
0 |
0 |
0 |
0 |
0 |
|
130 |
0 |
0 |
0 |
0 |
0 |
0 |
|
131 |
0 |
0 |
0 |
0 |
0 |
0 |
|
132 |
0 |
0 |
0 |
0 |
0 |
0 |
|
133 |
0 |
0 |
0 |
0 |
0 |
0 |
|
134 |
0 |
0 |
0 |
0 |
0 |
0 |
|
135 |
0 |
0 |
0 |
0 |
0 |
0 |
|
136 |
0 |
0 |
0 |
0 |
0 |
0 |
|
137 |
0 |
0 |
0 |
0 |
0 |
0 |
|
138 |
0 |
0 |
0 |
0 |
0 |
0 |
|
139 |
0 |
0 |
0 |
0 |
0 |
0 |
|
140 |
0 |
0 |
0 |
0 |
0 |
0 |
|
141 |
0 |
0 |
0 |
0 |
0 |
0 |
|
142 |
0 |
0 |
0 |
0 |
0 |
0 |
|
143 |
0 |
0 |
0 |
0 |
0 |
0 |
|
144 |
0 |
0 |
0 |
0 |
0 |
0 |
|
145 |
0 |
0 |
0 |
0 |
0 |
0 |
|
146 |
0 |
0 |
0 |
0 |
0 |
0 |
|
147 |
0 |
0 |
0 |
0 |
0 |
0 |
|
148 |
0 |
0 |
0 |
0 |
0 |
0 |
|
149 |
0 |
0 |
0 |
0 |
0 |
0 |
|
150 |
0 |
0 |
0 |
0 |
0 |
0 |
|
151 |
0 |
0 |
0 |
0 |
0 |
0 |
|
152 |
0 |
0 |
0 |
0 |
0 |
0 |
|
153 |
0 |
0 |
0 |
0 |
0 |
0 |
|
154 |
0 |
0 |
0 |
0 |
0 |
0 |
|
155 |
0 |
0 |
0 |
0 |
0 |
0 |
|
156 |
0 |
0 |
0 |
0 |
0 |
0 |
|
157 |
0 |
0 |
0 |
0 |
0 |
0 |
|
158 |
0 |
0 |
0 |
0 |
0 |
0 |
|
159 |
0 |
0 |
0 |
0 |
0 |
0 |
|
160 |
0 |
0 |
0 |
0 |
0 |
0 |
|
161 |
0 |
0 |
0 |
0 |
0 |
0 |
|
162 |
0 |
0 |
0 |
0 |
0 |
0 |
|
163 |
0 |
0 |
0 |
0 |
0 |
0 |
|
164 |
0 |
0 |
0 |
0 |
0 |
0 |
|
165 |
0 |
0 |
0 |
0 |
0 |
0 |
|
166 |
0 |
0 |
0 |
0 |
0 |
0 |
|
167 |
0 |
0 |
0 |
0 |
0 |
0 |
|
168 |
0 |
0 |
0 |
0 |
0 |
0 |
|
169 |
0 |
0 |
0 |
0 |
0 |
0 |
|
170 |
0 |
0 |
0 |
0 |
0 |
0 |
|
171 |
0 |
0 |
0 |
0 |
0 |
0 |
|
172 |
0 |
0 |
0 |
0 |
0 |
0 |
|
173 |
0 |
0 |
0 |
0 |
0 |
0 |
|
174 |
0 |
0 |
0 |
0 |
0 |
0 |
|
175 |
0 |
0 |
0 |
0 |
0 |
0 |
|
176 |
0 |
0 |
0 |
0 |
0 |
0 |
|
177 |
0 |
0 |
0 |
0 |
0 |
0 |
|
178 |
0 |
0 |
0 |
0 |
0 |
0 |
|
179 |
0 |
0 |
0 |
0 |
0 |
0 |
|
180 |
0 |
0 |
0 |
0 |
0 |
0 |
|
181 |
0 |
0 |
0 |
0 |
0 |
0 |
|
182 |
0 |
0 |
0 |
0 |
0 |
0 |
|
183 |
0 |
0 |
0 |
0 |
0 |
0 |
|
184 |
0 |
0 |
0 |
0 |
0 |
0 |
|
185 |
0 |
0 |
0 |
0 |
0 |
0 |
|
186 |
0 |
0 |
0 |
0 |
0 |
0 |
|
187 |
0 |
0 |
0 |
0 |
0 |
0 |
|
188 |
0 |
0 |
0 |
0 |
0 |
0 |
|
189 |
0 |
0 |
0 |
0 |
0 |
0 |
|
190 |
0 |
0 |
0 |
0 |
0 |
0 |
|
191 |
0 |
0 |
0 |
0 |
0 |
0 |
|
192 |
0 |
0 |
0 |
0 |
0 |
0 |
|
193 |
0 |
0 |
0 |
0 |
0 |
0 |
|
194 |
0 |
0 |
0 |
0 |
0 |
0 |
|
195 |
0 |
0 |
0 |
0 |
0 |
0 |
|
196 |
0 |
0 |
0 |
0 |
0 |
0 |
|
197 |
0 |
0 |
0 |
0 |
0 |
0 |
|
198 |
0 |
0 |
0 |
0 |
0 |
0 |
|
199 |
0 |
0 |
0 |
0 |
0 |
0 |
|
200 |
0 |
0 |
0 |
0 |
0 |
0 |
|
201 |
0 |
0 |
0 |
0 |
0 |
0 |
|
202 |
0 |
0 |
0 |
0 |
0 |
0 |
|
203 |
0 |
0 |
0 |
0 |
0 |
0 |
|
204 |
0 |
0 |
0 |
0 |
0 |
0 |
|
205 |
0 |
0 |
0 |
0 |
0 |
0 |
|
206 |
0 |
0 |
0 |
0 |
0 |
0 |
|
207 |
0 |
0 |
0 |
0 |
0 |
0 |
|
208 |
0 |
0 |
0 |
0 |
0 |
0 |
|
209 |
0 |
0 |
0 |
0 |
0 |
0 |
|
210 |
0 |
0 |
0 |
0 |
0 |
0 |
|
211 |
0 |
0 |
0 |
0 |
0 |
0 |
|
212 |
0 |
0 |
0 |
0 |
0 |
0 |
|
213 |
0 |
0 |
0 |
0 |
0 |
0 |
|
214 |
0 |
0 |
0 |
0 |
0 |
0 |
|
215 |
0 |
0 |
0 |
0 |
0 |
0 |
|
216 |
0 |
0 |
0 |
0 |
0 |
0 |
|
217 |
0 |
0 |
0 |
0 |
0 |
0 |
|
218 |
0 |
0 |
0 |
0 |
0 |
0 |
|
219 |
0 |
0 |
0 |
0 |
0 |
0 |
|
220 |
0 |
0 |
0 |
0 |
0 |
0 |
|
221 |
0 |
0 |
0 |
0 |
0 |
0 |
|
222 |
0 |
0 |
0 |
0 |
0 |
0 |
|
223 |
0 |
0 |
0 |
0 |
0 |
0 |
|
224 |
0 |
0 |
0 |
0 |
0 |
0 |
|
225 |
248 |
0 |
0 |
0 |
0 |
-4 |
|
226 |
247 |
0 |
0 |
0 |
0 |
-9 |
|
227 |
247 |
0 |
0 |
0 |
0 |
11 |
|
228 |
245 |
0 |
0 |
0 |
0 |
-5 |
|
229 |
244 |
0 |
0 |
0 |
0 |
0 |
|
230 |
243 |
0 |
0 |
0 |
0 |
5 |
|
231 |
241 |
0 |
0 |
0 |
0 |
-1 |
|
232 |
239 |
0 |
0 |
0 |
0 |
-4 |
|
233 |
237 |
0 |
0 |
0 |
0 |
-4 |
|
234 |
235 |
0 |
0 |
0 |
0 |
-2 |
|
235 |
233 |
0 |
0 |
0 |
0 |
2 |
|
236 |
230 |
0 |
0 |
0 |
0 |
0 |
|
237 |
227 |
0 |
0 |
0 |
0 |
1 |
|
238 |
223 |
0 |
0 |
0 |
0 |
-1 |
|
239 |
219 |
0 |
0 |
0 |
0 |
-1 |
|
240 |
215 |
0 |
0 |
0 |
0 |
0 |
|
241 |
210 |
0 |
0 |
0 |
0 |
0 |
|
242 |
204 |
0 |
0 |
0 |
0 |
-1 |
|
243 |
198 |
0 |
0 |
0 |
0 |
0 |
|
244 |
190 |
0 |
0 |
0 |
0 |
-1 |
|
245 |
183 |
0 |
0 |
0 |
0 |
1 |
|
246 |
173 |
0 |
0 |
0 |
0 |
0 |
|
247 |
163 |
0 |
0 |
0 |
0 |
0 |
|
248 |
151 |
0 |
0 |
0 |
0 |
0 |
|
249 |
137 |
0 |
0 |
0 |
0 |
0 |
|
250 |
121 |
0 |
0 |
0 |
0 |
0 |
|
251 |
104 |
0 |
0 |
0 |
0 |
0 |
|
252 |
83 |
0 |
0 |
0 |
0 |
0 |
|
253 |
59 |
0 |
0 |
0 |
0 |
0 |
|
254 |
30 |
0 |
0 |
0 |
0 |
0 |
|
255 |
0 |
0 |
0 |
0 |
0 |
0 |
This should help the user to set the ORx gain step to 1 dB for the desired ORx channel. Below is the test result on ADI EVB board with the 1dB step gain table for reference:
Test conditions:
Test result:
|
ORx Gain Index |
Power(dBFs) |
Step Error Between Current Gain Index and Previous Gain Index (dB) |
Step Error Between Current Gain Index and Max Gain Index 255(dB) |
|
255 |
-5.057 |
0 |
0 |
|
254 |
-5.945 |
0.112 |
0.112 |
|
253 |
-6.927 |
0.018 |
0.13 |
|
252 |
-7.898 |
0.029 |
0.159 |
|
251 |
-8.903 |
-0.005 |
0.154 |
|
250 |
-9.839 |
0.064 |
0.218 |
|
249 |
-10.783 |
0.056 |
0.274 |
|
248 |
-11.792 |
-0.009 |
0.265 |
|
247 |
-12.775 |
0.017 |
0.282 |
|
246 |
-13.721 |
0.054 |
0.336 |
|
245 |
-14.727 |
-0.006 |
0.33 |
|
244 |
-15.688 |
0.039 |
0.369 |
|
243 |
-16.658 |
0.03 |
0.399 |
|
242 |
-17.632 |
0.026 |
0.425 |
|
241 |
-18.637 |
-0.005 |
0.42 |
|
240 |
-19.615 |
0.022 |
0.442 |
|
239 |
-20.554 |
0.061 |
0.503 |
|
238 |
-21.556 |
-0.002 |
0.501 |
|
237 |
-22.524 |
0.032 |
0.533 |
|
236 |
-23.553 |
-0.029 |
0.504 |
|
235 |
-24.527 |
0.026 |
0.53 |
|
234 |
-25.533 |
-0.006 |
0.524 |
|
233 |
-26.531 |
0.002 |
0.526 |
|
232 |
-27.524 |
0.007 |
0.533 |
|
231 |
-28.487 |
0.037 |
0.57 |
|
230 |
-29.477 |
0.01 |
0.58 |
|
229 |
-30.482 |
-0.005 |
0.575 |
|
228 |
-31.494 |
-0.012 |
0.563 |
|
227 |
-32.518 |
-0.024 |
0.539 |
|
226 |
-33.515 |
0.003 |
0.542 |
|
225 |
-34.468 |
0.047 |
0.589 |
If the user find the ORx gain step error doesn’t match well with ADI EVB test result. To confirm the ORx gain table inside chip match with expectation. The user can call the API function adi_adrv9025_RxGainTableRead to read back the programmed ORx path gain table for a given channel.