Post Go back to editing

What are the main difference between ADRV9010 and ADRV9026.

What are the main difference between ADRV9010 and ADRV9026?.

Edit Notes

Updated.
[edited by: PVALAVAN at 11:16 AM (GMT -5) on 10 Dec 2020]
Parents
  • Main difference are,

    • Serdes lanes supported in ADRV9010 are 8 Lanes each in both direction where as ADRV9026 has only 4 lanes in both direction.
    • Max serdes rate supported by ADRV9010 is 16.22GHz and min is 1GHz. ADRV9026 max is 25 GHz and Min is 3GHz.
    • Frequency range for ADRV9010 is  650 to 3800MHz and for ADRV9026 is from 75 MHz to 6GHz.
Reply
  • Main difference are,

    • Serdes lanes supported in ADRV9010 are 8 Lanes each in both direction where as ADRV9026 has only 4 lanes in both direction.
    • Max serdes rate supported by ADRV9010 is 16.22GHz and min is 1GHz. ADRV9026 max is 25 GHz and Min is 3GHz.
    • Frequency range for ADRV9010 is  650 to 3800MHz and for ADRV9026 is from 75 MHz to 6GHz.
Children