Post Go back to editing

ADRV9009-ZU11EG FHM: inter-chip LO phase lands on discrete levels from hop to hop above ~4.5 GHz

Category: Software
Product Number: adrv9009-zu11eg
Software Version: Kuiper 11.2, kernel 6.1.70-284114-g2e8908932dfd, HDL hdl_2023_r2 (2156ac7e), ADRV9009 firmware 6.2.1 / API 3.6.2.1, libiio 0.26, pyadi-iio

Setup

  • ADRV9009-ZU11EG Rev.B, Kuiper 11.2, kernel 6.1.70-284114-g2e8908932dfd, HDL hdl_2023_r2 (2156ac7e), ADRV9009 firmware 6.2.1 / API 3.6.2.1, libiio 0.26, pyadi-iio adrv9009_zu11eg.
  • Profile: Rx RF BW 200 MHz, IQ rate 245.76 MSPS (default Kuiper device-tree profile).
  • An SMBV100B signal is split to the 4 Rx inputs (rx0A, rx1A on chip A; rx0B, rx1B on chip B) with matched, phase-stable R&S cables. All 4 channels are captured in the same DMA buffer.
  • Init on both chips: FHM with fhm-mode-enable-mcs-sync = 1 (range 150 MHz–6 GHz), initialize on chip A, mcs, init cals (Rx/Tx QEC, Rx phase correction), FHM enabled. Gain = slow_attack (AGC is unlikely to be the cause: rx0B and rx1B always jump together by the same amount, while rx0A–rx1A stays flat.). dig-clocks-rf-pll-phase-sync-mode = 3 (init + continuous tracking) is set on both chips before initialize and verified by readback afterwards.
  • LO frequencies are integer-N multiples of 30.72 MHz (153.6 … 5959.68 MHz, step 92.16 MHz). The same LO list is swept repeatedly (iterations). At each LO the generator is swept ±50 MHz, and the phase of each Rx relative to rx0A is measured. trx_lo is verified on both chips after every hop.
  • Hop trigger: I tested both the FHM GPIO trigger (both chips’ GPIOs toggled in a single register write) and the SPI trigger. The behaviour is similar with both.

Observation (plot attached: 30 iterations overlaid)

  • Same chip (rx0A–rx1A): ≈0° within a few degrees over the whole band.
  • Different chips (rx0A–rx0B, rx0A–rx1B): a linear ramp (~0.035°/MHz, ≈100 ps; external cabling is matched). Below ~4.5 GHz it is repeatable across iterations to a few degrees.
  • Above ~4.5 GHz, and especially above 5.5 GHz: for the same LO frequency, the inter-chip phase lands on 2–4 discrete levels about 10–15° apart, depending on the iteration (hop). Within a hop, the phase is stable across the whole –49.5 to +50 MHz generator sweep.
  • rx0B and rx1B jump together, by the same amount, while rx0A–rx1A does not. So the ambiguity looks like an LO phase offset of one whole chip relative to the other, not a per-channel effect.

Constraint
Re-running init cals or MCS after hops larger than 100 MHz is not possible: the application relies on fast FHM hops.
Questions

  1. With fhm-mode-enable-mcs-sync = 1 and RF PLL phase sync mode 3, should the inter-chip LO phase be deterministic after every FHM hop over 0.15–6 GHz?
  2. What can cause the LO phase between chips to land on discrete levels from hop to hop only at higher frequencies? VCO band/sub-band selection, LO divider, PLL lock behaviour in FHM? Can it be avoided by configuration or by the choice of LO frequencies?
  3. Is RF PLL phase sync (and its tracking) actually applied on FHM hops, or only on a regular (non-FHM) LO tune? Is any additional step needed?
  4. If it cannot be avoided, is the few-degree repeatability we see below ~4.5 GHz the best expected between two ADRV9009s in FHM?
Parents
  • With fhm-mode-enable-mcs-sync = 1 and RF PLL phase sync mode 3, should the inter-chip LO phase be deterministic after every FHM hop over 0.15–6 GHz?

    fhm-mode-enable-Mcs-sync = 1 and RF PLL phase synchronization help establish deterministic phase relationships but an FHM hop is fundamentally different from a fresh LO tune followed by a  complete synchronization sequence.
    ADRV9009 MCS provides deterministic timing alignment, but deterministic inter-chip LO phase is not guaranteed after each FHM LO retune. Following a hop, the RF PLL reacquires lock and the relative LO phase may change. Therefore phase coherence should be verified at the specific hop frequencies rather than assumed across the full 0.15-6 GHz range.
    What can cause the LO phase between chips to land on discrete levels from hop to hop only at higher frequencies? VCO band/sub-band selection, LO divider, PLL lock behaviour in FHM? Can it be avoided by configuration or by the choice of LO frequencies?
    Potential contributors include VCO band or sub-band selection, LO divider initialization, and PLL relock behavior during frequency hopping.
    This behavior is more likely at higher RF frequencies where different VCO regions or divider configurations are used.  A useful investigation is to correlate the phase states with the selected LO frequencies and VCO calibration results.

    Keep all hop frequencies within the same VCO band if possible.  Avoid  frequencies that force VCO band transitions.  Characterize the phase behavior versus LO frequency and look for correlation with VCO calibration results.
    Is RF PLL phase sync (and its tracking) actually applied on FHM hops, or only on a regular (non-FHM) LO tune? Is any additional step needed?

    RF PLL phase synchronization is applied during the RF PLL phase-sync procedure itself. An FHM hop is primarily a fast retune operation and does not inherently re-establish phase synchronization after each hop.
    If it cannot be avoided, is the few-degree repeatability we see below ~4.5 GHz the best expected between two ADRV9009s in FHM?

    A few degrees of repeatability below ~4.5 GHz would generally be considered good performance for two independent ADRV9009s operating in FHM. If the phase  remains within a few degrees after repeated hops and the behaviour degrades only when moving to higher frequencies.

  • Hi vanitha, thanks for the reply. It is consistent with the API documentation, where taliseFhmMode_t.enableMcsSync is described as MCS synchronization on FHM enable, so RF PLL phase sync is not repeated on each hop. Our application cannot leave FHM or re-run MCS/init cals between hops, so I’d like to understand which mechanism leaves the LO phase in discrete states, and whether any of these options can make it deterministic:

    1. Per-hop phase sync. I understand that inter-chip LO phase is not guaranteed after a hop because the RF PLL relocks. However, below ~4.5 GHz the relock is repeatable from hop to hop to within a few degrees, so the relock itself does not seem to be random. The uncertainty only appears above ~4.5 GHz, and as 2–4 discrete levels. What changes in that region: VCO core, VCO band, LO divider, or something else? Separately, is there an ARM command, or a SYSREF-based sequence, that re-runs RF PLL phase sync while staying in FHM? What does rfPllPhaseSyncMode = 3 (continuous tracking) do while FHM is active?

    2. VCO calibration in FHM. When FHM is entered with a scan range (fhmMinFreq_MHz/fhmMaxFreq_MHz, 150–6000 MHz here), does the ARM pre-calibrate and store VCO band/capacitor codes for the whole range, or does it run a fast VCO calibration on every hop? If it is per hop, can it be forced to reuse a stored result per frequency, so that the same LO always gets the same code? Would a narrower scan range, or several narrower ranges, change this?

    3. Register fields. Which fields in the RF synthesizer block (e.g. 0x0414 RF_SYNTH_CAL, 0x0417 RF_SYNTH_VCO_BAND_BYTE1 and neighbours) hold the VCO band and capacitor code selected after a hop? Can they be read back, or forced?

    4. PLL configuration. What are the RF PLL reference and PFD frequencies with the default ZU11EG profile (device clock 245.76 MHz)? Is relock phase after an FHM hop expected to be deterministic only for integer-N VCO/PFD ratios? If so, we can choose the LO grid accordingly.

    5. External LO. With one external LO distributed to both chips (rfPllUseExternalLo = 1), is FHM supported? In that mode, does MCS make the phase of the internal LO divider deterministic between chips?

    The discrete levels are 2–4 per LO, about 10–15° apart, and only appear above ~4.5 GHz (VCO above ~9 GHz). They are common to both channels of chip B and constant within a hop. Our current workaround is a per-hop reference-tone calibration, but we would prefer to make the LO phase deterministic if the firmware allows it.

    Thanks again.

Reply
  • Hi vanitha, thanks for the reply. It is consistent with the API documentation, where taliseFhmMode_t.enableMcsSync is described as MCS synchronization on FHM enable, so RF PLL phase sync is not repeated on each hop. Our application cannot leave FHM or re-run MCS/init cals between hops, so I’d like to understand which mechanism leaves the LO phase in discrete states, and whether any of these options can make it deterministic:

    1. Per-hop phase sync. I understand that inter-chip LO phase is not guaranteed after a hop because the RF PLL relocks. However, below ~4.5 GHz the relock is repeatable from hop to hop to within a few degrees, so the relock itself does not seem to be random. The uncertainty only appears above ~4.5 GHz, and as 2–4 discrete levels. What changes in that region: VCO core, VCO band, LO divider, or something else? Separately, is there an ARM command, or a SYSREF-based sequence, that re-runs RF PLL phase sync while staying in FHM? What does rfPllPhaseSyncMode = 3 (continuous tracking) do while FHM is active?

    2. VCO calibration in FHM. When FHM is entered with a scan range (fhmMinFreq_MHz/fhmMaxFreq_MHz, 150–6000 MHz here), does the ARM pre-calibrate and store VCO band/capacitor codes for the whole range, or does it run a fast VCO calibration on every hop? If it is per hop, can it be forced to reuse a stored result per frequency, so that the same LO always gets the same code? Would a narrower scan range, or several narrower ranges, change this?

    3. Register fields. Which fields in the RF synthesizer block (e.g. 0x0414 RF_SYNTH_CAL, 0x0417 RF_SYNTH_VCO_BAND_BYTE1 and neighbours) hold the VCO band and capacitor code selected after a hop? Can they be read back, or forced?

    4. PLL configuration. What are the RF PLL reference and PFD frequencies with the default ZU11EG profile (device clock 245.76 MHz)? Is relock phase after an FHM hop expected to be deterministic only for integer-N VCO/PFD ratios? If so, we can choose the LO grid accordingly.

    5. External LO. With one external LO distributed to both chips (rfPllUseExternalLo = 1), is FHM supported? In that mode, does MCS make the phase of the internal LO divider deterministic between chips?

    The discrete levels are 2–4 per LO, about 10–15° apart, and only appear above ~4.5 GHz (VCO above ~9 GHz). They are common to both channels of chip B and constant within a hop. Our current workaround is a per-hop reference-tone calibration, but we would prefer to make the LO phase deterministic if the firmware allows it.

    Thanks again.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.