Setup
- ADRV9009-ZU11EG Rev.B, Kuiper 11.2, kernel 6.1.70-284114-g2e8908932dfd, HDL hdl_2023_r2 (2156ac7e), ADRV9009 firmware 6.2.1 / API 3.6.2.1, libiio 0.26, pyadi-iio
adrv9009_zu11eg. - Profile: Rx RF BW 200 MHz, IQ rate 245.76 MSPS (default Kuiper device-tree profile).
- An SMBV100B signal is split to the 4 Rx inputs (rx0A, rx1A on chip A; rx0B, rx1B on chip B) with matched, phase-stable R&S cables. All 4 channels are captured in the same DMA buffer.
- Init on both chips: FHM with
fhm-mode-enable-mcs-sync = 1(range 150 MHz–6 GHz),initializeon chip A,mcs, init cals (Rx/Tx QEC, Rx phase correction), FHM enabled. Gain = slow_attack (AGC is unlikely to be the cause: rx0B and rx1B always jump together by the same amount, while rx0A–rx1A stays flat.).dig-clocks-rf-pll-phase-sync-mode = 3(init + continuous tracking) is set on both chips beforeinitializeand verified by readback afterwards. - LO frequencies are integer-N multiples of 30.72 MHz (153.6 … 5959.68 MHz, step 92.16 MHz). The same LO list is swept repeatedly (iterations). At each LO the generator is swept ±50 MHz, and the phase of each Rx relative to rx0A is measured.
trx_lois verified on both chips after every hop. - Hop trigger: I tested both the FHM GPIO trigger (both chips’ GPIOs toggled in a single register write) and the SPI trigger. The behaviour is similar with both.
Observation (plot attached: 30 iterations overlaid)

- Same chip (rx0A–rx1A): ≈0° within a few degrees over the whole band.
- Different chips (rx0A–rx0B, rx0A–rx1B): a linear ramp (~0.035°/MHz, ≈100 ps; external cabling is matched). Below ~4.5 GHz it is repeatable across iterations to a few degrees.
- Above ~4.5 GHz, and especially above 5.5 GHz: for the same LO frequency, the inter-chip phase lands on 2–4 discrete levels about 10–15° apart, depending on the iteration (hop). Within a hop, the phase is stable across the whole –49.5 to +50 MHz generator sweep.
- rx0B and rx1B jump together, by the same amount, while rx0A–rx1A does not. So the ambiguity looks like an LO phase offset of one whole chip relative to the other, not a per-channel effect.
Constraint
Re-running init cals or MCS after hops larger than 100 MHz is not possible: the application relies on fast FHM hops.
Questions
- With
fhm-mode-enable-mcs-sync = 1and RF PLL phase sync mode 3, should the inter-chip LO phase be deterministic after every FHM hop over 0.15–6 GHz? - What can cause the LO phase between chips to land on discrete levels from hop to hop only at higher frequencies? VCO band/sub-band selection, LO divider, PLL lock behaviour in FHM? Can it be avoided by configuration or by the choice of LO frequencies?
- Is RF PLL phase sync (and its tracking) actually applied on FHM hops, or only on a regular (non-FHM) LO tune? Is any additional step needed?
- If it cannot be avoided, is the few-degree repeatability we see below ~4.5 GHz the best expected between two ADRV9009s in FHM?