Post Go back to editing

Custom board. Synchronization of data between two ADRV9009 chips.

Thread Summary

The user is working on a custom board with two ADRV9009 transceivers and asks about JESD line restrictions for multi-chip synchronization. The final answer states that lanes should be aligned per ADRV9009 (per JESD link). Key points include ensuring SYSREF and DEVCLK are source synchronous, meeting setup and hold times for SYSREF, and receiving the rising edge of SYSREF during the same device clock cycle for proper synchronization.
AI Generated Content
Category: Hardware
Product Number: ADRV9009

Hello everyone! I've been working with two EVAL-ADRV9009 and ZCU102 boards. I managed to assemble one JESD for two ADRV9009s and achieve multi-chip synchronization. We're now creating our own board with two ADRV9009s. What are the restrictions on the JESD lines for multi-chip synchronization? (I need the signal to be phase-aligned). Is it possible to align the lines for only each ADRV9009 individually, or do all lines have to be length-aligned?