Post Go back to editing

FIFO on the Rx path of ADRV9009?

Category: Datasheet/Specs
Product Number: ADRV9009

Is there a FIFO on the Rx path of ADRV9009? Similar to that of the Tx path?

From UG-1295: "The FIFO depth can be checked in Register 0x15CE for Deframer 0 and in
Register 0x161E for Deframer 1." Is there something similar for the Framers A and B?

I have observed that the Rx latency can increase by 32 samples from reboot to reboot (randomly). Then I have changed .framerA.lmfcOffset from 31 to 15, and it seems it has solved the issue.

Parents Reply Children
No Data