ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
Is there a FIFO on the Rx path of ADRV9009? Similar to that of the Tx path?
From UG-1295: "The FIFO depth can be checked in Register 0x15CE for Deframer 0 and in
Register 0x161E for Deframer 1." Is there something similar for the Framers A and B?
I have observed that the Rx latency can increase by 32 samples from reboot to reboot (randomly). Then I have changed .framerA.lmfcOffset from 31 to 15, and it seems it has solved the issue.
Is there a FIFO on the Rx path of ADRV9009? Similar to that of the Tx path?
No.
have observed that the Rx latency can increase by 32 samples from reboot to reboot (randomly). Then I have changed .framerA.lmfcOffset from 31 to 15, and it seems it has solved the issue.
Is the issue solved?
If not, can you please provide test setup details?
Is there a FIFO on the Rx path of ADRV9009? Similar to that of the Tx path?
No.
have observed that the Rx latency can increase by 32 samples from reboot to reboot (randomly). Then I have changed .framerA.lmfcOffset from 31 to 15, and it seems it has solved the issue.
Is the issue solved?
If not, can you please provide test setup details?