ADRV9008-1
Recommended for New Designs
The receive path consists of two independent, wide bandwidth (BW), direct conversion receivers with state-of-the-art dynamic range. The complete receive...
Datasheet
ADRV9008-1 on Analog.com
Dear Team,
We are using the ADRV9008-1 Evaluation Board and would like to use a 200 MHz IBW bandwidth for scanning.
Could you please confirm whether a calibration is required for every scan? If calibration is required, what is the maximum time it would take to complete the calibration process?
Thank you for your support.
Regards,
P Prasanth
Yes, we would need to re-run the needed calibrations again.
As the frequency step change is more than 100 MHz, please follow below procedure.
Follow the " RF PLL FREQUENCY CHANGE PROCEDURE" from UG page 109.
Yes, we would need to re-run the needed calibrations again.
As the frequency step change is more than 100 MHz, please follow below procedure.
Follow the " RF PLL FREQUENCY CHANGE PROCEDURE" from UG page 109.