ADRV9009 maximum input power into RF port is 23 dBm (peak) according to datasheet, I suppose it is only for the short time.
What is absolute maximal signal into RF port continuously, I assume it doesn’t same ?
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
ADRV9009 maximum input power into RF port is 23 dBm (peak) according to datasheet, I suppose it is only for the short time.
What is absolute maximal signal into RF port continuously, I assume it doesn’t same ?
+23dbm is applicable for continuous signals as well . It is the maximum power that the chip can handle without damage, but performance is not guaranteed at such high powers.
Performance is guaranteed only till a maximum of -11dbm input power at RX port.

Thank you very much.
Thank you very much.