ADRV9009 maximum input power into RF port is 23 dBm (peak) according to datasheet, I suppose it is only for the short time.
What is absolute maximal signal into RF port continuously, I assume it doesn’t same ?
ADRV9009
Recommended for New Designs
The ADRV9009 is a highly integrated, radio frequency (RF), agile transceiver offering dual transmitters and receivers, integrated synthesizers, and digital...
Datasheet
ADRV9009 on Analog.com
ADRV9009 maximum input power into RF port is 23 dBm (peak) according to datasheet, I suppose it is only for the short time.
What is absolute maximal signal into RF port continuously, I assume it doesn’t same ?
+23dbm is applicable for continuous signals as well . It is the maximum power that the chip can handle without damage, but performance is not guaranteed at such high powers.
Performance is guaranteed only till a maximum of -11dbm input power at RX port.

Thank you very much.